cancel
Showing results for 
Search instead for 
Did you mean: 

activation of ST4SIM-300M and eSIM partners?

saharhaghdadi
Associate II

Hi , 

I recently acquired an ST4SIM-300M eSIM and I am unsure how the ST4SIM-300M should be activated initially.

I also watched your video about Remote SIM Provisioning using the Motive eSIM Secure Connect portal, and I would like to ask whether the activation and profile download for this SIM should be done through that portal.

Additionally, I would like to understand whether the SIM already contains a bootstrap profile by default. If so, how can I verify this from the device?

Finally, I would appreciate it if you could share a list of your eIM partners that support the ST4SIM-300M for testing purposes

2 REPLIES 2
Hannu-VS
Associate

Hello,

We are using also same eSIM. Did you got answer for this question ? My understanding is that eSIM is empty (based on another discussion in ST community forum). 

saharhaghdadi
Associate II

Hi,

I haven’t received a response from ST yet.

Based on what I’ve found so far (including other discussions), it seems that the ST4SIM-300M is delivered without a real bootstrap profile and only contains a dummy ICCID. If that is the case, it means there is no IPAe available on the card.

It looks like the only option would be to implement IPAd on the device side, which makes the integration more complex.