cancel
Showing results for 
Search instead for 
Did you mean: 

Will multiple TOF sensors (VL53L series specifically) in close proximity interfere with one another?

jds8086
Associate II

I am wanting to design a device that incorporates several TOF sensors in a uni-dimensional array for detecting an objects location. The sensors would have approximately 8mm of separation. Will they interfere with one another?

1 ACCEPTED SOLUTION

Accepted Solutions
John E KVAM
ST Employee

Generally no.

Each sensor will 'see' the other sensors as ambient light - and discount it.

But with too much ambient, the sensors don't work as well.

But unless you place them looking directly at each other at close distaces it should be OK.

Keep in mind these sensors have a 'field of view' and output a cone of light - instead of a 'dot'.

the VL53l5CX will provide you with an 8x8 array of answers. That might be exactly what you want.

  • john

If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.

View solution in original post

5 REPLIES 5
John E KVAM
ST Employee

Generally no.

Each sensor will 'see' the other sensors as ambient light - and discount it.

But with too much ambient, the sensors don't work as well.

But unless you place them looking directly at each other at close distaces it should be OK.

Keep in mind these sensors have a 'field of view' and output a cone of light - instead of a 'dot'.

the VL53l5CX will provide you with an 8x8 array of answers. That might be exactly what you want.

  • john

If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.

Thank you for your response.

So long as the sensors will report the closest object I believe there is a chance it will work out. I'm up for experimenting. But you do bring up a good point with the 8x8 sensor. Depending on it's field of view, that may work out very nice.

Here is a rudimentary drawing (top down view) of what i had in mind with the non-array sensors.

0693W00000aIcqyQAC.png 

John E KVAM
ST Employee

There are 2 sensors you want to consider. Both have identical silicon, are pin compatible and the code is very nearly identical.

the VL53L5CX (L5) has a 45x45 degree field of view.

The VL53L7CX (L7) has a 60x60 degree FoV.

The L7's diffractive optics are made the same way we make silicon chips. So the L7 is a touch less expensive than the L5.

Given the FoV the L5's zones are about 5 degrees.

The L7's zones are proportionally larger.

These sensors are our most expensive, but they are less expensive that multiple single-zone sensors.

  • john


If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.
jds8086
Associate II

Thank you

In regards to the L5 and L7, when using 4x4 resolution, is the FOV proportionally decreased or do the zones just cover a larger area?

John E KVAM
ST Employee

Zones are just larger. But with larger zones, you get more photon detectors per area. And with more detectors you can 'see' a bit farther and go a bunch faster.


If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.