2024-06-06 3:00 AM
I have used the VL53LCX Linux driver to operate the ToF sensor on the IMX8M Nano board, and the Linux driver is functioning correctly. However, I am encountering issues with implementing gesture recognition functionality. I have used the gesture recognition static library M7 Version, which cross-compiled successfully, but the gesture recognition is not working properly. Could you provide the appropriate .a file for the Linux architecture?
2024-06-06 10:24 AM
I could not tell from your description which processor you are using. Try to find out which MCU you have. Something like ARM-Cortex M4.
With that you can select one of the pre-compiled libraries.
If you can't find one that supports your particular MCU then write back.
- john
2024-06-06 11:35 PM
Hey John,
The IMX8M Nano comes equipped with the following processor configuration:
IMX8MN working on the Android (Android 12) framework and an Integrated TOF Driver within the AOSP Linux layer, Hence, The applications run on the Cortex-A53 processor. In order to ensure proper functionality, would I require a .a file specifically for the Cortex-A53 architecture?
I have attached application files here for the reference.