2024-07-09 5:09 AM - last edited on 2024-07-09 5:56 AM by Peter BENSCH
I am using the VL53L4CD sensor board very similar to https://www.sparkfun.com/products/18993 with my application. I am using the modified version of https://github.com/stm32duino/VL53L4CD driver on the Raspberry Pico board.
I am using the both the xshut and INTR pins.
I am able to read the sensor ID and load the default configuration without any issues. However, the call to
Solved! Go to Solution.
2024-07-09 9:48 AM
That's crazy - The first read is of a defined hardware register. and it sure looks like it was read correctly.
So, your reads work!
But the other lines write the data as bytes, words and long-words. And you are reading back zeros.
QED, your writes are failing to actually write.
At this point you must debug the I2C write themselves. It's got to be in there somewhere.
If you don't write, you can't configure the chip - or start it.
Which is what you are seeing.
2024-07-09 6:26 AM
If you've gotten to SensorInit, you have been communicating with the chip quite a bit. But it's clearly not right, and the first opportunity to know this is the 'are you done yet' is failing.
I'm going to guess that it's a byte-swap or work-swap issue. Because it always is.
#define I2C_TEST
#ifdef I2C_TEST
int rd_write_verification( uint16_t dev, uint16_t addr, uint32_t expected_value)
{
VL53L4CD_Error Status = VL53L4CD_ERROR_NONE;
uint8_t bytes[4];
uint16_t words[2];
uint32_t dword;
int i;
for (i=0; i<4; i++){ VL53L4CD_RdByte((uint16_t)dev, addr+i, &bytes[i]); }
for (i=0; i<2; i++){ VL53L4CD_RdWord(dev, addr+i*2, &words[i]); }
Status = VL53L4CD_RdDWord(dev, addr, &dword);
printf("expected = %8x,\n",(unsigned int)expected_value);
printf("read_bytes = %2x, %2x, %2x, %2x\n", bytes[0],bytes[1],bytes[2],bytes[3]);
printf("read words = %4x, %4x\n",words[0],words[1]);
printf("read dword = %8x\n",(unsigned int)dword);
if((bytes[0]<<24 | bytes[1]<<16 | bytes[2]<<8 | bytes[3]) != expected_value) return (-1);
if((words[0]<<16 | words[1]) != expected_value) return (-1);
if(dword != expected_value) return(-1);
return Status;
}
#define REG 0x3A
void i2c_test(uint16_t dev)
{
VL53L4CD_Error Status = VL53L4CD_ERROR_NONE;
int err_count = 0;
uint8_t buff[4] = {0x11,0x22,0x33,0x44};
int i=0;
Status = rd_write_verification(dev, 0x10f, 0xebaa10ff); // verify the Chip ID works
Status += VL53L4CD_WrDWord(dev, REG, 0xffeeddcc); // check WrDWord
if (rd_write_verification(dev, REG, 0xffeeddcc) <0) err_count++;
Status += VL53L4CD_WrWord(dev, REG, 0x5566); // check WrWord
Status += VL53L4CD_WrWord(dev, REG+2, 0x7788);
if (rd_write_verification(dev, REG, 0x55667788) <0) err_count++;
for (i=0; i<4; i++){ VL53L4CD_WrByte (dev, REG+i, buff[i]); }
if (rd_write_verification(dev, REG,0x11223344) <0) Status++;
if (Status > 0)
{
printf("i2c test failed - please check it. Status = %d\n", Status);
}
}
#endif
Put this bit of code in just after you think your sensor is booted.
It simply writes bytes and reads words and longwords.
It's my guess that because you had some writes 'backwards' the sensor was just not understanding the commands you were giving.
I could be wrong of course, but it's easy enough to check.
- john
2024-07-09 9:10 AM
2024-07-09 9:48 AM
That's crazy - The first read is of a defined hardware register. and it sure looks like it was read correctly.
So, your reads work!
But the other lines write the data as bytes, words and long-words. And you are reading back zeros.
QED, your writes are failing to actually write.
At this point you must debug the I2C write themselves. It's got to be in there somewhere.
If you don't write, you can't configure the chip - or start it.
Which is what you are seeing.