2023-04-08 2:18 AM
I have attached a couple of histograms from same object and from different distances. Distances are embedded in filename visible in image (top bar). Problem is peak position doesn’t change. I understand depth data is spread across three bins only. But how possibly does the peaks only happen at one position.
NB: the extra peaks on the far right for some of the histograms I presume to be as result of reflection.
can anyone help clarify how to see objects distances let’s say in meters (as max distance is 4m) ?
also if this is not possible I’d like some clarification about why.
v++
2023-04-18 12:58 AM
Hello,
histograms are internal data used by our patented algorithms inside our driver to compute ranging values. ST will not disclose the patented algorithms
Anne
2023-04-18 11:03 AM
Hi, I suggest you please read post again. There is NO request to disclose ST patented algorithms. It’s an open question and you’re allowed to pass if you don’t know the answer
2023-04-21 11:48 AM
Each group of 3 in those histograms is a target. In the images with two peaks, you have 2 targets.
In that first image, I'm thinking you are seeing something like your hand, and then the ceiling behind the hand.
You get the results from the sensor along with the histogam. I suggest you compare those results with your histogram data.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.