cancel
Showing results for 
Search instead for 
Did you mean: 

VL53L1 interrupt problem

joh.5
Associate II

Hello.

Isn't the period of interrupt not in timing budget?

When tested indoors, the period of the interrupt is the timing budget.

However, when testing outdoors, the interrupt cycle is irregular.

If you look at UM2133 - Rev 6 page 11, what is reported when a target is not detected.

If it is not detected, it should be reported as not detected, but no interrupt is generated.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Anne BIGOT
ST Employee

I am assuming you have a distance threshold.

Indoors, whenever that threshold is met, you get a nice consistent interrupt.

Outdoors, in bright sun light, the sensor doesn't work as well. And it may be that the threshold can not be met in those light conditions so the sensor just gives up.


Our community relies on fruitful exchanges and good quality content. You can thank and reward helpful and positive contributions by marking them as 'Accept as Solution'. When marking a solution, make sure it answers your original question or issue that you raised.

ST Employees that act as moderators have the right to accept the solution, judging by their expertise. This helps other community members identify useful discussions and refrain from raising the same question. If you notice any false behavior or abuse of the action, do not hesitate to 'Report Inappropriate Content'