2022-03-21 8:31 AM
2022-03-29 6:35 AM
There is only one driver for the VL53L5CX. They should be the same.
2022-03-28 4:37 PM
The files should be the same, but there might have been modifications to comply with the X-CUBE format. Can you give me some examples of different code?
2022-03-29 3:45 AM
Thank you for the answer. Sorry, I put the question wrong. I wanted to know if the API used in the X-CUBE-TOF1 examples was different from the one used in the ULD driver examples. The doubt arises from the fact that for some sensors (VL53L1X) a "Full" version and an Ultra Lite version were available, so I was wondering if maybe this difference could exist also in the case of the VL53L5CX
2022-03-29 6:35 AM
There is only one driver for the VL53L5CX. They should be the same.
2022-03-31 4:37 AM
Hi @John E KVAM ,
related to the VL53L5CX API in the X-CUBE-TOF1 package, I saw that effectively are the same as the ULD driver for VL53L5CX. I don't understand in which way they are used in the X-CUBE-TOF1 package. I will try to explain my doubt.
Trying to study the CUSTOM application for F401RE in this package I was not able to see the "link" between the structure RANGING_SENSOR_Drv_t
typedef struct
{
int32_t (*Init)(void *);
int32_t (*DeInit)(void *);
int32_t (*ReadID)(void *, uint32_t *);
int32_t (*GetCapabilities)(void *, void *);
int32_t (*ConfigProfile)(void *, void *);
int32_t (*ConfigROI)(void *, void *);
int32_t (*ConfigIT)(void *, void *);
int32_t (*GetDistance)(void *, void *);
int32_t (*Start)(void *, uint8_t);
int32_t (*Stop)(void *);
int32_t (*SetAddress)(void *, uint16_t);
int32_t (*GetAddress)(void *, uint16_t *);
int32_t (*SetPowerMode)(void *, uint32_t);
int32_t (*GetPowerMode)(void *, uint32_t *);
} RANGING_SENSOR_Drv_t;and the various function defined in the ultra-lite driver files. But when I go in debug mode I see that effectively this structure is linked to the ULD. For example, the field "Init" is linked to the function:
int32_t VL53L5CX_Init(VL53L5CX_Object_t *pObj)
{
int32_t ret;
if (pObj == NULL)
{
ret = VL53L5CX_INVALID_PARAM;
}
else if (pObj->IsInitialized != 0U)
{
ret = VL53L5CX_ERROR;
}
else if (vl53l5cx_init(&pObj->Dev) != VL53L5CX_STATUS_OK)
{
ret = VL53L5CX_ERROR;
}
else
{
pObj->IsRanging = 0U;
pObj->IsBlocking = 0U;
pObj->IsContinuous = 0U;
pObj->IsAmbientEnabled = 0U;
pObj->IsSignalEnabled = 0U;
pObj->IsInitialized = 1U;
ret = VL53L5CX_OK;
}
return ret;
}which in turn invokes the function vl53l5cx_init defined in the ULD for VL53L5CX. Can you or someone please explain to me how this link is established?
Unfortunately I haven't been able to figure it out on my own. Thanks again for the answers and suggestions you have given me these days. They helped me a lot
2022-04-01 6:06 AM
Somewere in your app code you will find the following sentence:
VL53L5A1_RANGING_SENSOR_Init(device);If you debug your code you will see this functions finally calls
[Your custom]RANGING_SENSOR_Drv->Init(VL53L5A1_RANGING_SENSOR_CompObj[Instance])And as you have cited RANGING_SENSOR_Drv_t is a struct type of function pointers. And bear in mind in vl53l5cx.h you have a symmetrical declaration of function pointers:
typedef struct
{
int32_t (*Init)(VL53L5CX_Object_t *);
int32_t (*DeInit)(VL53L5CX_Object_t *);
int32_t (*ReadID)(VL53L5CX_Object_t *, uint32_t *);
int32_t (*GetCapabilities)(VL53L5CX_Object_t *, VL53L5CX_Capabilities_t *);
int32_t (*ConfigProfile)(VL53L5CX_Object_t *, VL53L5CX_ProfileConfig_t *);
int32_t (*ConfigROI)(VL53L5CX_Object_t *, VL53L5CX_ROIConfig_t *);
int32_t (*ConfigIT)(VL53L5CX_Object_t *, VL53L5CX_ITConfig_t *);
int32_t (*GetDistance)(VL53L5CX_Object_t *, VL53L5CX_Result_t *);
int32_t (*Start)(VL53L5CX_Object_t *, uint32_t);
int32_t (*Stop)(VL53L5CX_Object_t *);
int32_t (*SetAddress)(VL53L5CX_Object_t *, uint32_t);
int32_t (*GetAddress)(VL53L5CX_Object_t *, uint32_t *);
int32_t (*SetPowerMode)(VL53L5CX_Object_t *, uint32_t);
int32_t (*GetPowerMode)(VL53L5CX_Object_t *, uint32_t *);
} VL53L5CX_RANGING_SENSOR_Drv_t;MYCUSTOM_RANGING_SENSOR_Drv = (RANGING_SENSOR_Drv_t *) &VL53L5CX_RANGING_SENSOR_Driver;