2022-10-03 2:18 AM
Hi all,
I'm trying to get the GUI to perform Xtalk calibration, but every attempt so far returns the error 'Error from ULD: XTalk error, invalid parameter provided'.
I've tried altering the default parameters in various combinations but no luck so far.
Does anyone have a clue as to what I'm missing here?
Arie
2022-10-03 7:33 AM
in order to do crosstalk, the absolute ideal condition would be to point the sensor into some completely open area. Nothing within a good 5 feet. I use my desk looking up at a ceiling. (make sure there is noting in the FoV,)
Then set the parameters to 5% reflectance an as big a distance as tool will allow. I use 999.
But the real trick is that you actually need a coverglass. Without a coverglass, you do get an error.
And once calibrated, be sure to check the "CoverGlass On" box. Otherwise the calibration is not taken into account.
2022-10-03 7:56 AM
Thanks John,
This was with the cover glass placed and the box ticked, but it may have had to do with the spacer I had in between. I started with a 1mm spacer. I tried again with a 0.25mm spacer and a distance of 999, and now it calibrated just fine.
2022-10-03 8:14 AM
Give it another try. I used it with both layers of an anti-static bag as a coverglass and although the bag makes a really awful coverglass, you do get a result.