cancel
Showing results forĀ 
Search instead forĀ 
Did you mean:Ā 

STA8089 GA - Cannot activate IF pins to verify front-end functionality

Armin Choopani
Associate II

I hope you have a great day

Iā€™m Armin Choopani, Studying Electrical Engineering. Iā€™ve been assigned a project which is setting up GNSS module. I decided to use the STA8089 GA IC. Iā€™ve designed a matching circuit for its LNA pin. But Unfortunately I cannot verify its functionality (Front-end gain and NF), because I cannot find appropriate command to activate IF pins. Iā€™ve read all NMEA file. But there wasnā€™t any command related to IF pins. I was wondering if you could help me to find this command. This problem halted my whole project, because I cannot verify anything.

Thank you all

This discussion is locked. Please start a new topic to ask your question.
14 REPLIES 14
Armin Choopani
Associate II

Hi Francesco

Thank God you are back again =)

Yes, I have satellites issue again. Sometimes IC detects a satellite and sometimes no (But it just detect a satellite, not more. I have a Teseo module which detects lots of satellites with the same antenna and at the same place). Also when my IC detects a satellite, the CN0 fluctuates enormously (from 20 to 35).

Another point about hardware mask or signature string (which I don't know what they are exactly). On my IC it is written "BB" but when I use "$PSTMGETSWVER,255", it says that the IC mask is BD. Does this make any problem?

Best Regards

Armin

Francesco Virlinzi
ST Employee

Ciao Armin

> it says that the IC mask is BD

This is not an issue.

Your wafer-die is newer then DD, at the end it's a good chip.

> But it just detect a satellite, not more

It's very strange, it sees only one satellite.

> Also when my IC detects a satellite, the CN0 fluctuates enormously (from 20 to 35).

It could be an issue related the TCXO.

If not covered with a shield (or similar) it can introduce fluctuations in the RF part.

You could try to cover the TCXO and generally check if some-one is introducing noice in your platform

Ciao

Francesco

Armin Choopani
Associate II

Dear Francesco

Again nothing interesting. I have tried different shieldings, but it just detects one satellite (satellite number 31 with CN0=34) while My Teseo III detects satellite number 31 with CN0=39. Even when the CN0 of two different satellites are same (based on Teseo III output), my IC just detects one of the satellites.

I don't know where I should search for the problem or problems! Digital section or RF section or both.

Best Regards

Armin

Francesco Virlinzi
ST Employee

Ciao

> I don't know where I should search for the problem or problems! Digital section or RF section or both.

I'm sorry to say you should check both.

It could be an issue in the power supply or something wrong in the pcb.

Regards

Francesco

Armin Choopani
Associate II

Ciao Francesco

I check and see what I can do. By the way, thanks for your informative responses. I learned a lot from them.

Best Regards

Armin