2023-08-24 11:12 AM
Hi,
How does one set the max fix rate of the Teseo Liv3f GPS to a floating point number? The UM2229 documentation mentioned the parameter value must be expressed in hexadecimal format for any integer value and decimal for any not integer value. The allowable max fix rate value is "> 0.1".
Here is the definition of the set parameter function:
$PSTMSETPAR,<ConfigBlock><ID>,<param_value>[,<mode>]*<checksum><cr><lf>
Thanks.
2023-08-30 02:18 AM
The following scripts will set Fix-Rate @ 10Hz:
$PSTMCFGCLKS,0,0,0
$PSTMSETPAR,1303,0.1,0
$PSTMSAVEPAR
$PSTMSRR
Regards
Francesco
2023-08-30 03:44 AM
Not sure that was the question. I think the OP understood 0.1 was 100 ms / 10 Hz
Suspect the question related to broader numbers, with longer delays and sub-Hz