cancel
Showing results for 
Search instead for 
Did you mean: 

Does having a coin cell battery give a significantly quicker fix?

JOrta
Associate II

Is there a significant improvement in having a fix quicker by having the coin cell battery?

or can i live without it..

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Francesco Virlinzi
ST Employee

Hi

VBAT (supplied with coin cell battery) manages the internal SRAM and RTC.. they are used to validated or not the previous dowloaded satellite data.

At the end if in your design you plan to swtich_off VCC/VCC_IO and you want avoid a cold-boot on each repowering the VBAT supply (coin cell battery) is mandatory to guarantee a TTFF of 4s instead of 32s.

Hope this helps.

Regards

Francesco