Subject | Author | Posted | |
---|---|---|---|
Dear support team, is there Reference schematic, register description or a Eval board for the FD...
| 2022-12-30 12:28 AM | ||
Hello I have an audio card based on the STA 350BW it has 4 amplified mono outputs. I wou...
| 2022-12-11 07:01 AM | ||
I'm using STEVAL-IME013V1 ultrasound pulser IC evaluation board. I'm using the board as 8 channel p...
| 2022-12-06 01:54 AM | ||
I'm using STEVAL-IME013V1 ultrasound pulser IC evaluation board. I'm using the board as 8 channel...
| 2022-12-01 01:14 AM | ||
I am starting my first project with the STUW813000. I don't seem to find a clear answer to the foll...
| 2022-11-29 04:05 AM | ||
Dear Friends. We have manufactured a circuit for the STuW81300. We have conected it to an Arduino D...
| 2022-11-28 07:52 AM | ||
Hi. I am simulating rhf200 using TINA Tool. The data sheet shows that the input voltage range is ab...
| 2022-11-22 04:23 AM | ||
2022-11-21 08:08 AM | |||
i have set enables 1,2,3 and 4 as 1100 which is address 2 , but for some reason the speaker is not ...
| 2022-09-30 04:25 AM | ||
I have several "mystery" failures of STN1HN60 in one of our commercial product ranges. There is n...
| 2022-09-29 06:58 PM | ||
Needed Detailed Thermal Model for TDA7803A which includes Die, Solder balls etc., and their materia...
| 2022-09-21 11:48 PM | ||
2022-09-05 02:23 AM | |||
I have an application where I'm using a 0.001 ohm sense resistor and the TS2010H Current Sense Ampl...
| 2022-09-01 10:57 AM | ||
Good afternoon.... I am looking into using an STA540 in a power amp design for a single supply 4 o...
| 2022-08-25 02:02 PM | ||
STuW81300 I designed a device with STuW81300. PLL locked. I received output power like in the ...
| 2022-08-08 06:07 AM | ||
Sometime ago, I've built-up a simple single-sided test brd where I could plug-in a TDA72xx series f...
| 2022-08-02 09:49 PM | ||
2022-08-01 02:15 AM | |||
I am using the STuW81300 as LO generator to generate 12GHz LO. Although I am able to get the freque...
| 2022-07-29 12:40 AM | ||
Hello, I want to send data to the DAC with the I2S protocol (assume we are sending an array) and se...
| 2022-07-26 11:25 PM | ||
Need an operational amplifier for the video signal booster, with bandwidth >85MHz, able to work to ...
| 2022-07-07 02:13 AM |