Subject | Author | Posted | |
---|---|---|---|
hello I'm currently using the LPS22DF pressure transducer, which can withstand up to 22,000 g, but...
| 2023-11-13 5:27 AM | ||
Can i reduce the sensitivity ("sensitivity": 1) for a microphone (IMP23ABSU) for it not to reach th...
| 2023-11-11 12:10 PM | ||
Hello. I would like to make a new project for the "SensorTile.box PRO" board using STM32CubeIDE...
| 2023-11-03 10:55 AM | ||
I'm currently using MEMS MP34DT06JTR audio sensor with STM32L431KBU6TR Mcu. I'm facing issue in rec...
| 2023-10-13 12:20 AM | ||
Use the cubeProgram tool to burn the MPU, whether the USB of the MPU must use USB-OTG mode?
| 2023-10-11 5:06 AM | ||
We have used PM8805 tr POE PD IC. And design is very similar to one of the evolution board. Its not...
| 2023-10-05 11:39 AM | ||
Hello, I am experiencing a port fault issue with my Steval-MKI109v3 board which is equipped with a...
| 2023-10-03 7:16 AM |