Subject | Author | Posted | |
---|---|---|---|
I'm working with the VL53L1X as part of my bachelors projekt. In that regard I'd like to explain to...
| 2019-11-14 04:59 AM | ||
when hand held device is flat i get roll and pitch degree -2 and +2. during pitch measurement :...
| 2019-11-13 11:36 PM | ||
Hi, I hope you can help me with this one. My problem is on line 127 I'm making an array of stru...
| 2019-11-13 01:35 AM | ||
Hi, I'm using the LSM6DSL AWT to get interrupts in Y-axis when the angle goes above or below the...
| 2019-11-12 09:05 AM | ||
I am extracting LSM6DSL's data at FIFO rate 833 Hz and I set the SPI rate at 10MHz which is the max...
| 2019-11-02 09:28 PM | ||
I configured the device and I am able to read XYZ data by polling the status register 0x27 and read...
| 2019-10-30 06:25 AM | ||
Background: I want to calculate tilt angle of my resting device (g is the only acceleration presen...
| 2019-10-29 02:42 AM | ||
Hello, I apologize in advance for my long post, and ignorance when it comes to interpreting thi...
| 2019-10-28 12:18 PM | ||
I had an error // not supported by motherboard // when connect STEVAL-MKI197V1 to UNICO like the i...
| 2019-10-22 04:14 AM | ||
Hello Team, We want to test self-test mode in LIS2DH12TR. We have followed below application ...
| 2019-10-22 03:31 AM | ||
My LIS3DH is not outputting any data, its displaying a value of 127, any idea why
| 2019-10-21 06:18 AM | ||
2019-10-11 02:17 AM | |||
I think that this board can measure precision current. So I want to use full range of current. ...
| 2019-10-10 03:13 AM | ||
Hi, I'm trying to get the heading direction from the compass of LSM303AGR, I'm getting the X,Y,Z d...
| 2019-10-08 02:30 AM | ||
From what I understand, the slave device I want to communicate with has many addressed registers th...
| 2019-10-05 12:50 AM | ||
I am using the V6180X Satel boards and occasionally when I power up the sensor it remains non-funct...
| 2019-09-26 09:17 AM | ||
I need help with the vl53l0x sensor and stm32f103 board if anyone can help me with programming or a...
| 2019-09-20 07:42 PM | ||
Hi, I'm Looking for a suitable design pattern to reliably handle interrupts from the embedded fun...
| 2019-09-18 11:53 PM | ||
May I know what information will be read back from 0xc0 and 0xc1 from L53L1X?
| 2019-09-04 07:51 PM | ||
According to STMicroelectronics guide on github STMems_Android_Sensor_HAL_Input I'm unable to find ...
| 2019-09-04 05:46 AM |