Subject | Author | Posted | |
---|---|---|---|
Hi, We are testing BLE advertisement intervals in noisy environment(where there are multiple BLE d...
| 2023-05-25 11:01 PM | ||
Hello, I would like to power an STM32WLE5 with two voltage levels: VBAT: 2 series AA batteries...
| 2023-05-25 1:37 AM | ||
Hello, I want to use STM32WB55 with Zephyr to communicate via openthread network. Which FW Version...
| 2023-05-24 2:41 AM | ||
Hello I set the variable uint8_t test as test = test + 1 in main.c and send this variable vi...
| 2023-05-24 1:59 AM | ||
2023-05-24 12:14 AM | |||
I am using the "BLE_DataThroughput" sample code on Nucleo-WB55RG, and sending 240 bytes to Windows ...
| 2023-05-22 11:41 AM | ||
Hi, im using a loRawan module based on STM32WLE5 chip. i would like to know how i can save an eve...
| 2023-05-22 7:57 AM | ||
Hi All, Currently I am working on STM32WLE5CCU6 + RAK3172 using STM32CubeIDE. So I am checking s...
| 2023-05-22 2:17 AM | ||
I want to know how to design a PCB board about stm32wb55cc serial ic ,and should it need a antenna...
| 2023-05-19 8:02 PM | ||
Hello everyone, I am trying to do tone calculator. I am using DSP , ADC ,DMA and timer for sampling...
| 2023-05-18 1:17 PM | ||
Greetings, I am working on the LoRaWAN Project and facing issues in updating RTC from a server/U...
| 2023-05-17 5:54 AM | ||
Why on my LRWAN3 node card, when I power it externally on the +E5V tab, the LoRa card doesn't trans...
| 2023-05-17 2:22 AM | ||
Hi, I am using a STM32WB55, and a third party IMU device. I used the P2P client demo code to start...
| 2023-05-16 3:16 PM | ||
I am developing a FreeRTOS project with around 12 tasks, many of which use the open thread ot* func...
| 2023-05-15 8:03 PM | ||
Hello everyone I produce devices on the WB55CG with a BLE stack. There is a working firmware wi...
| 2023-05-15 4:03 AM | ||
I am using stm32wl55jc1. I want to use accelerometer at 50khz and microphone at 2khz (2048). I am t...
| 2023-05-14 11:43 PM | ||
Unluckily, I haven't found indications as to which of this functions to use for a basic transmit/...
| 2023-05-14 3:26 PM | ||
How to write our own STM32WB BD Address when production? Is there any tool or APIs of Windows to co...
| 2023-05-11 7:43 PM | ||
Hi all ! Does anyone know if it's possible to port SPI Emulator to the STM32WB5MMG family ? (or ...
| 2023-05-09 4:10 PM | ||
I am getting the following errors when debuging the project from the package. I have the standard p...
| 2023-05-09 1:45 AM |