| Subject | Author | Posted | |
|---|---|---|---|
|
I'm using the STM32F407T6 for the first time and would like to be able to communicate with my compu...
| 2024-11-07 4:57 AM | ||
|
Hi All, I was looking for an EMI Filter for SD card interface in STM32H753VI design. I am going ...
| 2024-11-07 1:35 AM | ||
|
Hello, Custom Board Development with STM32U585 Microcontroller We have developed a custom board f...
| 2024-11-05 2:06 AM | ||
|
Hi, I'm working on POST using X-cube STL in stm32h745zit3 using IAR 9.30.1 version, while flashing...
| 2024-11-04 10:51 PM | ||
|
I recently saw your presentation of HSO in motor control. I have a couple of questions: 1) Is the...
| 2024-11-04 5:35 AM | ||
|
Hi, I'm using STM32G474 to drive my BLDC motor, i want to trig low-side phase current sensing ADC ...
| 2024-11-01 10:59 AM | ||
|
Hi all, I am trying to activate SDADC on my custom designed board to measure a couple of analog vo...
| 2024-10-31 3:44 AM | ||
|
Hello! This is the first time im using NOR Flash so bear with me :) Question #1 I screwed up an...
| 2024-10-31 3:08 AM | ||
|
Hi I am using X-CUBE-DPOWER to set the parameters for my Buck converter operating conditions on a...
| 2024-10-30 10:17 PM | ||
|
This is a problem about the STM32H745XI-Disco control external AD5791 through SPI. When using Debug...
| 2024-10-30 6:46 AM | ||
|
I am working on the development of a Bootloader for one of our projects. We are encountering an iss...
| 2024-10-27 11:40 PM | ||
|
Hello. Is there an example F/W for STEVAL-ESC001V1 or X-NUCLEO-IHM08M1 that is SPL compatible? I ...
| 2024-10-27 7:35 PM | ||
|
Dear STM Community I am reaching out on behalf of our development team, as we are in the process o...
| 2024-10-27 1:22 AM | ||
|
I'm trying to program an STM32U5 microcontroller with Open On-Chip Debugger 0.12.0+dev-00597-ga5a21...
| 2024-10-26 8:19 AM | ||
|
Hello, I'm trying communication between stm32G0 as I2C slave and a rapsberry pi 5 as master. o...
| 2024-10-25 2:31 AM | ||
|
I'm working on a STM32G473RCT6 CPU with 256K Flash in dualbank mode. looking for information on ad...
| 2024-10-24 7:20 AM | ||
|
For my current project, I am seeking recommendations for the most suitable STM32 microcontroller se...
| 2024-10-22 10:10 PM | ||
|
I’m new to the STM32L4 community and currently working on an assignment for my studies, using the S...
| 2024-10-21 12:22 PM | ||
|
Hi, the device have some kind of limitation on the usage of DMA? What I did: 1 - Implemented DMA0...
| 2024-10-20 11:46 PM | ||
|
I have an STM32F103VET6 with multiple DMA Channels like UART2_RX, ADC, UART3_RX, UART3_TX, all at d...
| 2024-10-20 10:35 PM |