cancel
Showing results for 
Search instead for 
Did you mean: 

Why does my NanoEdge AI Studio training process get stuck at this interface, when I'm using it to train the benchmark model?

PP_Developer
Visitor

Hi Supporter:

     I attempted to train a model using NanoEdge AI Studio,Some errors occurred!

    first,I create a NC-class project (ps:I haven't connected the development board. I'm just using the computer for simulation.)

    

PP_Developer_0-1737601732403.png

PP_Developer_1-1737601754876.png

add signal

PP_Developer_4-1737601902548.png

 

PP_Developer_3-1737601890632.png

benchmark

PP_Developer_5-1737601948861.png

When I clicked "Start," the screen stuck on this page and stayed there all day, only to be closed through the task manager.

PP_Developer_6-1737602025957.png

What's the problem?

 

1 ACCEPTED SOLUTION

Accepted Solutions
Julian E.
ST Employee

Hello @PP_Developer ,

 

Everything seems correct at first glance.

Please try to restart your computer to make sure everything related to NanoEdge is closed

Uninstall NanoEdge

Install NanoEdge again.

 

Sometime, during the installation / update, there are issues due to non-closed elements.

 

Please keep me updated.

 

Have a good day,

Julian


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

3 REPLIES 3
Julian E.
ST Employee

Hello @PP_Developer ,

 

Everything seems correct at first glance.

Please try to restart your computer to make sure everything related to NanoEdge is closed

Uninstall NanoEdge

Install NanoEdge again.

 

Sometime, during the installation / update, there are issues due to non-closed elements.

 

Please keep me updated.

 

Have a good day,

Julian


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

The outcome is the same, whether it is restarting the computer or reinstalling the software.

I guess there might be the following several possibilities.

1.Network issue. Is it because I can't access your model library from my end? Could you provide me with a URL or domain name of the model library so that I can ping it?

2.Regarding the issue of permissions, I applied for the serial code through the email. Is it because of insufficient permissions?

3.Regarding the computer configuration issue, do you have any requirements for the configuration of the computer? For example, regarding the memory?

Hello,

 

Can you send me the log files in a zip please:

  • Click on the icon as in the screenshot in the bottom left corner.

JulianE_0-1737624695214.png

 

Network issue may cause error but later in the process.

You don't need permission

As for requirements make sure to have free disk space but that's it...

 

Julian 


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.