2022-08-31 3:42 AM
Hey. I’m quite new to microcontrollers and also have this question. I’ve checked all the solutions but didn’t work. I need help.
I am using STM32F4291-DISC1 board and validating an LSTM model on target. I got the following error: E200(ValidationError): stm32: Unable to bind the STM AI runtime with "prediction_model" c-model:
connection to "serial:COM4:115200"/"COM4:115200" run-time fails
E801(HwIOError): Invalid firmware - COM4:115200
I believe it is a single core I don’t have Cortex-M7 option to switch.
Also, I’m using STM32CubeIDE. After compiling and running the code, the RAM and FLASH usage are:
Is it normal? I am wondering if it is because the model is not download into the board.
2022-08-31 7:35 AM
Hello @HLU.1 ,
May be this post helps you: Anyone faced this type of issue and got resolved
Imen