2024-08-24 11:20 PM
I want to run Cube AI Model zoo examples on STM32H745. The current example in Model zoo is for STM32H747 with a display, I can replace the display and print the output on UART.
Is there an example or tutorial that explains the changes required to run AI on STM32H745? I would appreciate a detailed answer with a guide, as I am new to STM MCUs.
Development kits: NUCLEO-144 STM32H745ZI EVAL BRD
2024-09-02 12:43 AM
Hello,
As of today, the application examples contained in the STM32 Model Zoo are supporting only two STM32 boards:
- The STM32H747 DK board, and
- The STM32H743 Nucleo board.
Thank you.
Julien.