cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H747I-Disco Board Trying to run custom model- error 'ai_layer_conv2d'

Sarvesh1
Associate

'ai_layer_conv2d' {aka 'struct ai_layer_conv2d_'} has no member named 'in_ch_format'

'ai_layer_conv2d' {aka 'struct ai_layer_conv2d_'} has no member named 'out_ch_format'

 

Also i am trying to run a object detection model in which i want to glows LEDs based on the position of the object on the screen based on the coordinates of bounding box. Can anyone help in that.

3 REPLIES 3
dogg
Associate III

Have you figured what creates this error?

Julian E.
ST Employee

Hello @Sarvesh1 ,

Can you describe the steps you followed, what you are doing please. Where do you get this error?

What version of X-Cube-AI are you using? Try using the last available.

 

Have a good day,

Julian

 


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Hi,

I am following this tutorial to use my own image recognition model with the STM32H747I-DISCO board. I have already ran the demos and they seem to work fine.

So I even followed the colab part and made the model with the flowers.

I have made the adjustments for the NT35510 screen that I have.

I have done the Updating to a newer version of X-CUBE-AI part in the tutorial successfully.

The tflite model is successfully generated and i copy the network files to my person detection project and when I try to build the project I get the same errors as above.
Can you please run the example as the tutorial suggests to see if it works?

thanks

STM cube version 1.16.1

X-CUBE-AI version 9.1.0