2024-07-30 06:28 AM
I want to use X CUBE AI VERSION 7.3.0. I have installed the package with correct version but when I try to use it pops a saying "Please select local zip file for X-Cube-AI stm32ai utilities". I cannot find the zip file anywhere where should be located. I have also tried version 9.0.0 and no tab opens up in that version. But I need to use 7.3.0. I am attaching a screenshot as well.
2024-07-30 07:34 AM
Hello,
It probably means X-CUBE-AI plugin was not able to contact distant server in order to download it.
Based on your screenshot, you can install it manually from the zip.
Here are the steps:
- Go to https://www.st.com/en/embedded-software/x-cube-ai.html
- Click or Scroll down to "Get Software"
- Look for the row corresponding to the column "X-CUBE-AI-Win" if you are on Windows.
- Select version "7.3.0" and follow the next steps in your browser.
It should start a ZIP download labeled as "en.x-cube-ai-windows_v7.3.0.zip"
- Unzip it, it contains another ZIP named "stm32ai-windows-7.3.0.zip"
- From STM32CubeMX, browse to this folder and select this zip
Hope it helps.
Best regards,
Yanis
2024-07-31 02:33 AM
Thank you for reply the version problem was resolved but it when I generate code with it for the model. The middleware and and Debug folder is not generated with the required files. Due to which it gives me error when I build the project. I am attaching the screenshots for your understanding. Is that a problem with X Cube AI version 7.3.0. Because I generate the code with version 9.0.0 as well which is ok. But I specifically want to use version 7.3.0.