2025-03-26 4:12 AM
Some errors occurred during the model conversion process. I have provided my model file below.
Cube-AI report :NOT IMPLEMENTED: Gemm with channel first A input is not supported
It seems to be caused by an inability to handle the transposed data, but how do I resolve this issue? Or is the transpose operator unusable?
Solved! Go to Solution.
2025-03-27 6:21 AM
Hello @Nephalem ,
Yes indeed, it is hard to tell.
In the X Cube AI menu, you can click setting and set --verbosity 3:
But I don't think it is enough.
What you should do is use stedgeai.exe manually.
When you do a validate in X Cube AI, it literally does:
stedgeai.exe generate --model your_model --target stm32n6 --st-neural-art
So you can open a bash terminal and do this manually but you also need to first do:
export _DEBUG=2
to have more logs.
Have a good day,
Julian
2025-03-26 8:07 AM
Hello @Nephalem,
It seems there is also an issue with the Gemm layers in your model.
If we take a look at the first one:
With:
And:
So, your operation effectively becomes: 𝑌=(𝐴×𝐵𝑇)+𝐶
You can try to replace the Gemm layers by with basic layers such as transpose, matmul and add.
Something like this:
import torch
# Define the inputs
A = torch.randn(1, 144) # Shape (1, 144)
B = torch.randn(128, 144) # Shape (128, 144)
C = torch.randn(128) # Shape (128,)
# Perform equivalent Gemm operation using matmul, transpose, and add
Y = torch.matmul(A, B.T) + C # B.T gives shape (144, 128), matmul gives (1, 128)
# Print result shape to verify
print(Y.shape) # Should be (1, 128)
Please double check with the Gemm pytorch documentation that this is correct.
Have a good day,
Julian
2025-03-26 11:40 PM
Hello @Julian E.
Following your instructions, I solved that problem, but now I've encountered a new issue。
TOOL ERROR: list index out of range
I have a few other questions. For example, how can I make CUBE-AI print longer debug logs? It's really hard to tell exactly which array is causing the out-of-bounds error from just this single line of error message. Thank you, and I hope you have a great day
2025-03-27 6:21 AM
Hello @Nephalem ,
Yes indeed, it is hard to tell.
In the X Cube AI menu, you can click setting and set --verbosity 3:
But I don't think it is enough.
What you should do is use stedgeai.exe manually.
When you do a validate in X Cube AI, it literally does:
stedgeai.exe generate --model your_model --target stm32n6 --st-neural-art
So you can open a bash terminal and do this manually but you also need to first do:
export _DEBUG=2
to have more logs.
Have a good day,
Julian
2025-03-27 6:43 AM
Hello @Julian E.
I tried it, but didn’t get any output in the folder. Where should I add the export _DEBUG=2 parameter? My device uses the STM32F4 series, and the interface is slightly different from yours, though not significantly. If possible, could you help me analyze where the array out-of-bounds error mentioned in the model occurs? I would greatly appreciate it. Alternatively, could you share the CUBE-AI debug report for me to review?
Thank you
hope you have a nice day!