Skip to main content
Associate
January 26, 2025
Solved

MLC functionality on MKSBOX1v1

  • January 26, 2025
  • 2 replies
  • 880 views

I have this board with STM32L4R9 and I used CubeMX and Unico-GUI tools to generate a decision tree for MLC in .ucf format. I used a python script to convert this to C uint8_t array as follows:

 

const uint8_t lsm6dsox_ucf[] = {
0x10, 0x00,
0x11, 0x00,
0x01, 0x80,
0x05, 0x00,
0x17, 0x40,
0x02, 0x11,
...
};

In the generated main function I use my function to upload this array to MLC:
void lsm6dsox_load_ucf_via_spi()
{
size_t ucf_size = sizeof(lsm6dsox_ucf) / sizeof(lsm6dsox_ucf[0]);

for (size_t i = 0; i < ucf_size; i += 2)
{
uint8_t reg = lsm6dsox_ucf[i]; // Register address
uint8_t value = lsm6dsox_ucf[i + 1]; // Register value

lsm6dsox_spi_write(reg, value);
HAL_Delay(10);
}

HAL_Delay(10);
}
 
void lsm6dsox_spi_write(uint8_t reg, uint8_t value)
{
// The first byte is the register address (with MSB cleared for write).
uint8_t tx_data[2] = {reg & 0x7F, value};

// Pull CS low to select the sensor
HAL_GPIO_WritePin(CS_LSM6DSOX_GPIO_Port, CS_LSM6DSOX_Pin, GPIO_PIN_RESET);

// Send data over SPI
HAL_SPI_Transmit(&hspi1, tx_data, 2, HAL_MAX_DELAY);

// Pull CS high to deselect the sensor
HAL_GPIO_WritePin(CS_LSM6DSOX_GPIO_Port, CS_LSM6DSOX_Pin, GPIO_PIN_SET);

// Small delay for stability
HAL_Delay(10);
}
 
after which I constantly pool the 0x70 register for decision tree 1 output but it never changes
uint8_t lsm6dsox_spi_read(uint8_t reg)
{
uint8_t tx_data = reg | 0x80;
uint8_t rx_data = 0;

// Pull CS low to select the sensor
HAL_GPIO_WritePin(CS_LSM6DSOX_GPIO_Port, CS_LSM6DSOX_Pin, GPIO_PIN_RESET);

// Transmit the register address and receive the response
HAL_SPI_Transmit(&hspi1, &tx_data, 1, HAL_MAX_DELAY);
HAL_SPI_Receive(&hspi1, &rx_data, 1, HAL_MAX_DELAY);

// Pull CS high to deselect the sensor
HAL_GPIO_WritePin(CS_LSM6DSOX_GPIO_Port, CS_LSM6DSOX_Pin, GPIO_PIN_SET);

return rx_data;
}
 
When I manually upload the .ucf file using Unico-GUI the gesture detection works and I get changes in the status register on the UI. What am I doing wrong?
This topic has been closed for replies.
Best answer by Federica Bossi

Hi @bigcoronagigachad ,

We suggest to use MEMS Studio instead of Unico.
We see no errors in the code, you could convert the UCF using the “C code generation” function of Unico (or better MEMS Studio).

Also, can you in general read and write? For example, can you read the who am I? Can you turn on the accelerometer and read the data?
To read 0x70 (MLC0_SRC), are you first writing 0x01 to 0x80 to get access to that register? And then you reset it to 0x00 after doing the read to restore access to the main registers?

2 replies

Federica Bossi
Federica BossiBest answer
ST Technical Moderator
February 14, 2025

Hi @bigcoronagigachad ,

We suggest to use MEMS Studio instead of Unico.
We see no errors in the code, you could convert the UCF using the “C code generation” function of Unico (or better MEMS Studio).

Also, can you in general read and write? For example, can you read the who am I? Can you turn on the accelerometer and read the data?
To read 0x70 (MLC0_SRC), are you first writing 0x01 to 0x80 to get access to that register? And then you reset it to 0x00 after doing the read to restore access to the main registers?

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
Associate
March 15, 2025

My problem was I eventually used C code generation function of Unico but I did not adjust the load_ucf_file_via_spi function to take into account the new data structure, also writing to 0x80 register first to access MLC0_SRC was missing