2025-03-14 8:07 AM
I want to train one of the pretrained AI models (lets say i choose yamnet), on my own data. I want to use mimii dataset which consists of different industrial equipment sound files in .wav format in normal working condition and anomalous working condition. I only want to test on valve type sound so only two classes normal and anomalous sound type are needed. How do i convert the format to esc-50 format as said in the tutorial, i see that there are .csv files as well as .wav files in the esc-50 dataset.
2025-03-14 8:31 AM - edited 2025-03-14 8:32 AM
Hello @jzzunn ,
Thank you for your question, here is what you need to do:
Put all WAV files in a single folder (e.g., audio/).
Ensure each file is in a consistent format (e.g., 44.1 kHz, mono, 16-bit WAV).
Then you need to create a meta.csv. Each row in meta.csv should contain:
Example of meta.csv
filename,category
0001.wav,normal
0002.wav,abnormal
0003.wav,normal
0004.wav,abnormal
...
Then to retrain the model, follow this tutorial:
Have a good day,
Julian
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.