cancel
Showing results for 
Search instead for 
Did you mean: 

stm32ai-modelzoo-services-main benchmarking error!

fanronghua0123456
Associate III

[INFO] : Quantization complete.
[INFO] : Evaluating the quantized model using validation_set...
INFO: Created TensorFlow Lite XNNPACK delegate for CPU.
100%|██████████| 36/36 [05:01<00:00, 8.37s/it]
[INFO] : Accuracy of quantized model on validation_set = 98.17%
[INFO] : Evaluation complete.
[INFO] : Using the local download of STM32Cube.AI. Link to download https://www.st.com/en/embedded-software/x-cube-ai.html
[INFO] : Starting the model memory footprints estimation...
[WARN] : STM32Cube.AI installed version 2.1.0 does not match the version specified in user_config.yaml file 10.1.0 !
[INFO] : STM32Cube.AI version 2.1.0 used.
Error executing job with overrides: []
Traceback (most recent call last):
File "C:\st\stm32ai-modelzoo-services-main\.venv\lib\site-packages\clearml\binding\hydra_bind.py", line 230, in _patched_task_function
return task_function(a_config, *a_args, **a_kwargs)
File "C:\st\stm32ai-modelzoo-services-main\image_classification\stm32ai_main.py", line 399, in main
process_mode(mode=mode, configs=cfg, train_ds=train_ds, valid_ds=valid_ds, quantization_ds=quantization_ds,
File "C:\st\stm32ai-modelzoo-services-main\image_classification\stm32ai_main.py", line 315, in process_mode
chain_tqeb(cfg=configs, train_ds=train_ds, valid_ds=valid_ds, quantization_ds=quantization_ds, test_ds=test_ds)
File "C:\st\stm32ai-modelzoo-services-main\image_classification\stm32ai_main.py", line 233, in chain_tqeb
benchmark(cfg=cfg, model_path_to_benchmark=quantized_model_path, credentials=credentials)
File "C:\st\stm32ai-modelzoo-services-main\common\benchmarking\common_benchmark.py", line 58, in benchmark
_stm32ai_benchmark(footprints_on_target=board,
File "C:\st\stm32ai-modelzoo-services-main\common\benchmarking\common_benchmark.py", line 549, in _stm32ai_benchmark
_analyze_footprints(offline=offline, results=cloud_res, stm32ai_output=stm32ai_output, inference_res=inference_res, target_mcu=target_mcu)
File "C:\st\stm32ai-modelzoo-services-main\common\benchmarking\common_benchmark.py", line 80, in _analyze_footprints
with open(os.path.join(stm32ai_output, 'network_report.json'), 'r') as f:
FileNotFoundError: [Errno 2] No such file or directory: 'C:\\st\\stm32ai-modelzoo-services-main\\image_classification\\src\\experiments_outputs\\2025_07_25_09_01_04/stm32ai_files\\network_report.json'

Set the environment variable HYDRA_FULL_ERROR=1 for a complete stack trace.

进程已结束,退出代码为 1

1 ACCEPTED SOLUTION

Accepted Solutions

I think I have solved this problem. I just need to replace the X-CUBE-AI version with 10.0.0

View solution in original post

7 REPLIES 7
fanronghua0123456
Associate III

network_report.json file  have not been  created!

fanronghua0123456
Associate III

i append some log in common_benchmark.py.


# Run generate command locally
command = f"{path_to_stm32ai} generate --target stm32 -m {model_path} -v 0 --output {stm32ai_output} --workspace {stm32ai_output} --optimization {optimization}"
# command = f"{path_to_stm32ai} generate --target stm32n6 -m {model_path} --st-neural-art user_neuralart.json"
print("command00 = {}".format(command))
args = shlex.split(command, posix="win" not in sys.platform)
print("command01 = {}".format(command))
subprocess.run(args, env=new_env, check=True)
print("command02 = {}".format(command))
except subprocess.CalledProcessError as e:
raise TypeError(
f"Received: stm32ai.path_to_stm32ai={path_to_stm32ai}. Please specify a correct path to STM32Cube.AI!") from e

return stm32ai_output



[INFO] : STM32Cube.AI version 2.1.0 used.
command00 = C:/Users/Administrator/STM32Cube/Repository/Packs/STMicroelectronics/X-CUBE-AI/10.1.0/Utilities/windows/stedgeai.exe generate --target stm32 -m ./pretrained_models/best_model.h5 -v 0 --output C:\st\stm32ai-modelzoo-services-main_bak\stm32ai-modelzoo-services-main\image_classification\src\experiments_outputs\2025_07_25_14_33_22/stm32ai_files --workspace C:\st\stm32ai-modelzoo-services-main_bak\stm32ai-modelzoo-services-main\image_classification\src\experiments_outputs\2025_07_25_14_33_22/stm32ai_files --optimization balanced
command01 = C:/Users/Administrator/STM32Cube/Repository/Packs/STMicroelectronics/X-CUBE-AI/10.1.0/Utilities/windows/stedgeai.exe generate --target stm32 -m ./pretrained_models/best_model.h5 -v 0 --output C:\st\stm32ai-modelzoo-services-main_bak\stm32ai-modelzoo-services-main\image_classification\src\experiments_outputs\2025_07_25_14_33_22/stm32ai_files --workspace C:\st\stm32ai-modelzoo-services-main_bak\stm32ai-modelzoo-services-main\image_classification\src\experiments_outputs\2025_07_25_14_33_22/stm32ai_files --optimization balanced
command02 = C:/Users/Administrator/STM32Cube/Repository/Packs/STMicroelectronics/X-CUBE-AI/10.1.0/Utilities/windows/stedgeai.exe generate --target stm32 -m ./pretrained_models/best_model.h5 -v 0 --output C:\st\stm32ai-modelzoo-services-main_bak\stm32ai-modelzoo-services-main\image_classification\src\experiments_outputs\2025_07_25_14_33_22/stm32ai_files --workspace C:\st\stm32ai-modelzoo-services-main_bak\stm32ai-modelzoo-services-main\image_classification\src\experiments_outputs\2025_07_25_14_33_22/stm32ai_files --optimization balanced
Error executing job with overrides: []
Traceback (most recent call last):
File "C:\st\stm32ai-modelzoo-services-main\.venv\lib\site-packages\clearml\binding\hydra_bind.py", line 230, in _patched_task_function
return task_function(a_config, *a_args, **a_kwargs)
File "C:\st\stm32ai-modelzoo-services-main_bak\stm32ai-modelzoo-services-main\image_classification\stm32ai_main.py", line 399, in main
process_mode(mode=mode, configs=cfg, train_ds=train_ds, valid_ds=valid_ds, quantization_ds=quantization_ds,
File "C:\st\stm32ai-modelzoo-services-main_bak\stm32ai-modelzoo-services-main\image_classification\stm32ai_main.py", line 309, in process_mode
benchmark(cfg=configs)
File "C:\st\stm32ai-modelzoo-services-main_bak\stm32ai-modelzoo-services-main\common\benchmarking\common_benchmark.py", line 58, in benchmark
_stm32ai_benchmark(footprints_on_target=board,
File "C:\st\stm32ai-modelzoo-services-main_bak\stm32ai-modelzoo-services-main\common\benchmarking\common_benchmark.py", line 551, in _stm32ai_benchmark
_analyze_footprints(offline=offline, results=cloud_res, stm32ai_output=stm32ai_output, inference_res=inference_res, target_mcu=target_mcu)
File "C:\st\stm32ai-modelzoo-services-main_bak\stm32ai-modelzoo-services-main\common\benchmarking\common_benchmark.py", line 80, in _analyze_footprints
with open(os.path.join(stm32ai_output, 'network_report.json'), 'r') as f:
FileNotFoundError: [Errno 2] No such file or directory: 'C:\\st\\stm32ai-modelzoo-services-main_bak\\stm32ai-modelzoo-services-main\\image_classification\\src\\experiments_outputs\\2025_07_25_14_33_22/stm32ai_files\\network_report.json'

Set the environment variable HYDRA_FULL_ERROR=1 for a complete stack trace.




Hello @fanronghua0123456,

 

Can you share the yaml you used? And the model if possible?

Else, do you see this issue with other models?

 

Have a good day,

Julian


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Julian E.

Thanks  for your reply,  and  The attachment is my configuration file .I think this is not a model issue, but rather a configuration issue that has caused the absence of the output file "network_report.json"

I think I have solved this problem. I just need to replace the X-CUBE-AI version with 10.0.0

Hello @fanronghua0123456,

 

Yes, it seems that you don't have the version 2.1.0 installed on your pc.

For now I would suggest sticking to the 10.0.0 version for testing. But if you can, please use the last version available as each version fixes bugs.

 

Have a good day,

Julian


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Julian,

Thanks for your help.