2024-06-22 01:42 PM
Hi,
I've joined introductory imbedded AI course on Udemy, unfortunately it is more than 4 years old using AI pack version 3.4.0 and I cannot get support from the instructor.
Please find attached a presentation with screen shots of all steps used to generate the project and compiler messages after each corrective action until I can no longer do anything and stuck.
Thank you in advance
2024-06-22 01:43 PM
2024-06-22 01:45 PM
2024-06-23 12:45 AM
I've followed instructions in the following link:
and build project with the same errors as per compiler3.txt.
Then tried to 'clean' the project rather than 'build' and voila all errors disappeared as per attached file compiler4.txt. Is that it?
2024-06-23 01:07 AM