Skip to main content
Associate
November 8, 2024
Solved

Cannot analyze ONNX model: INTERNAL ERROR: 'numpy.ndarray' object has no attribute 'get_shape_map'

  • November 8, 2024
  • 2 replies
  • 1112 views

Hi all, I am trying to benchmark a TCN (causal cnn)-model on an STM32u5, however, when using any of the AI-Tools (online, CubeIDE or CLI), the analysis step fails with the output:

 

 

ST Edge AI Core v1.0.0-19894
INTERNAL ERROR: 'numpy.ndarray' object has no attribute 'get_shape_map'

 

 

Which is sadly not helpful. The model is attached, it was converted to onnx from pytorch (or rather fastai) using opset 13. It should take an input of 1x500x1 (bs x 1DSample x channels) and give an output of the same shape.

I would be happy to get any pointers on what I can do to fix this, thank you!

This topic has been closed for replies.
Best answer by Julian E.

Hello @GfbGoesBrr ,

 

I have confirmed it is an error with the current public version of ST Edge AI Core. It is fixed in the upcoming version that should come out mid-December. 

 

Unfortunately, you can't do anything until the new version of the ST Edge AI Core comes out...

 

Have a good day,

Julian

2 replies

Julian E.
Julian E.Best answer
ST Technical Moderator
November 14, 2024

Hello @GfbGoesBrr ,

 

I have confirmed it is an error with the current public version of ST Edge AI Core. It is fixed in the upcoming version that should come out mid-December. 

 

Unfortunately, you can't do anything until the new version of the ST Edge AI Core comes out...

 

Have a good day,

Julian

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Associate
November 20, 2024

Thank you for the effort!

I removed a somewhat custom part of the model definition, now it works already.

 

Side note: Giving the option to have more usefull logs would be appreciated, I tried setting the verbosity to different values but it does not change the behavior. Online and in Cube IDE the verbosity is always set to a specific level too, even if I try to overwrite it using the user flag field.