2026-01-13 4:13 AM
Hi,
based on the ST example where the 640kB RAM is splitted into 2 * 320kB for secure/non-secure application, I want to change this to 32kB/608kB for secure/non-secure app.
After modification of the linker files for the secure/non-secure app, the non-secure app runs into an hardfault right at the start. The error is that some ns access is done in secure area in SRAM1 (at address 0x2001f840).
I first started the project on the STM32H563 eval board and simply copied the settings of MPU and GTZC over to the STM32H562. These settings are working on the STM32H563, so I can properly jump there into the non-secure app.
Are there any difference in setting the memory areas for secure/non-secure/priviledged feature?
Here are the settings.
linkerfile non-secure:
define symbol __ICFEDIT_region_RAM_start__ = 0x20008000;
define symbol __ICFEDIT_region_RAM_end__ = 0x2009FFFF;
linkerfile secure:
define symbol __ICFEDIT_region_RAM_start__ = 0x30000000;
define symbol __ICFEDIT_region_RAM_end__ = 0x30007FFF;
void MPU_Config(void)
{
MPU_Region_InitTypeDef MPU_InitStruct = {0};
MPU_Attributes_InitTypeDef MPU_AttributesInit = {0};
/* Disables the MPU */
HAL_MPU_Disable();
/** Initializes and configures the Region 0 and the memory to be protected
*/
MPU_InitStruct.Enable = MPU_REGION_ENABLE;
MPU_InitStruct.Number = MPU_REGION_NUMBER0;
MPU_InitStruct.BaseAddress = 0x0C018400;
MPU_InitStruct.LimitAddress = 0x0C01DFFF;
MPU_InitStruct.AttributesIndex = MPU_ATTRIBUTES_NUMBER0;
MPU_InitStruct.AccessPermission = MPU_REGION_PRIV_RO;
MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_ENABLE;
MPU_InitStruct.IsShareable = MPU_ACCESS_NOT_SHAREABLE;
HAL_MPU_ConfigRegion(&MPU_InitStruct);
/** Initializes and configures the Region 1 and the memory to be protected
*/
MPU_InitStruct.Number = MPU_REGION_NUMBER1;
MPU_InitStruct.BaseAddress = 0x30000000;
MPU_InitStruct.LimitAddress = 0x30007FFF;
MPU_InitStruct.AttributesIndex = MPU_ATTRIBUTES_NUMBER1;
MPU_InitStruct.AccessPermission = MPU_REGION_PRIV_RW;
HAL_MPU_ConfigRegion(&MPU_InitStruct);
...static void MX_GTZC_S_Init(void)
{
/* USER CODE BEGIN GTZC_S_Init 0 */
/* USER CODE END GTZC_S_Init 0 */
MPCWM_ConfigTypeDef MPCWM_Area_Desc = {0};
MPCBB_ConfigTypeDef MPCBB_Area_Desc = {0};
/* USER CODE BEGIN GTZC_S_Init 1 */
/* USER CODE END GTZC_S_Init 1 */
MPCWM_Area_Desc.AreaId = GTZC_TZSC_MPCWM_ID1;
MPCWM_Area_Desc.Offset = 0x0;
MPCWM_Area_Desc.Length = 0x02000000;
MPCWM_Area_Desc.Attribute = GTZC_TZSC_MPCWM_REGION_NSEC|GTZC_TZSC_MPCWM_REGION_NPRIV;
MPCWM_Area_Desc.Lock = GTZC_TZSC_MPCWM_LOCK_OFF;
MPCWM_Area_Desc.AreaStatus = ENABLE;
if (HAL_GTZC_TZSC_MPCWM_ConfigMemAttributes(OCTOSPI1_BASE, &MPCWM_Area_Desc) != HAL_OK)
{
Error_Handler();
}
MPCBB_Area_Desc.SecureRWIllegalMode = GTZC_MPCBB_SRWILADIS_ENABLE;
MPCBB_Area_Desc.InvertSecureState = GTZC_MPCBB_INVSECSTATE_NOT_INVERTED;
MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[0] = 0xFFFFFFFF;
MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[1] = 0xFFFFFFFF;
MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[2] = 0x00000000;
MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[3] = 0x00000000;
MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[4] = 0x00000000;
MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[5] = 0x00000000;
MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[6] = 0x00000000;
MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[7] = 0x00000000;
MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[8] = 0x00000000;
MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[9] = 0x00000000;
MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[10] = 0x00000000;
MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[11] = 0x00000000;
MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[12] = 0x00000000;
MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[13] = 0x00000000;
MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[14] = 0x00000000;
MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[15] = 0x00000000;
MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[0] = 0xFFFFFFFF;
MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[1] = 0xFFFFFFFF;
MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[2] = 0xFFFFFFFF;
MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[3] = 0xFFFFFFFF;
MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[4] = 0xFFFFFFFF;
MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[5] = 0xFFFFFFFF;
MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[6] = 0xFFFFFFFF;
MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[7] = 0xFFFFFFFF;
MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[8] = 0xFFFFFFFF;
MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[9] = 0xFFFFFFFF;
MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[10] = 0xFFFFFFFF;
MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[11] = 0xFFFFFFFF;
MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[12] = 0xFFFFFFFF;
MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[13] = 0xFFFFFFFF;
MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[14] = 0xFFFFFFFF;
MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[15] = 0xFFFFFFFF;
MPCBB_Area_Desc.AttributeConfig.MPCBB_LockConfig_array[0] = 0x00000000;
if (HAL_GTZC_MPCBB_ConfigMem(SRAM1_BASE, &MPCBB_Area_Desc) != HAL_OK)
{
Error_Handler();
}
MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[0] = 0x00000000;
MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[1] = 0x00000000;
MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[2] = 0x00000000;
MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[3] = 0x00000000;
MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[0] = 0xFFFFFFFF;
MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[1] = 0xFFFFFFFF;
MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[2] = 0xFFFFFFFF;
MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[3] = 0xFFFFFFFF;
MPCBB_Area_Desc.AttributeConfig.MPCBB_LockConfig_array[0] = 0x00000000;
if (HAL_GTZC_MPCBB_ConfigMem(SRAM2_BASE, &MPCBB_Area_Desc) != HAL_OK)
{
Error_Handler();
}
MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[0] = 0x00000000;
MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[1] = 0x00000000;
MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[2] = 0x00000000;
MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[3] = 0x00000000;
MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[4] = 0x00000000;
MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[5] = 0x00000000;
MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[6] = 0x00000000;
MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[7] = 0x00000000;
MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[8] = 0x00000000;
MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[9] = 0x00000000;
MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[10] = 0x00000000;
MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[11] = 0x00000000;
MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[12] = 0x00000000;
MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[13] = 0x00000000;
MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[14] = 0x00000000;
MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[15] = 0x00000000;
MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[16] = 0x00000000;
MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[17] = 0x00000000;
MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[18] = 0x00000000;
MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[19] = 0x00000000;
MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[0] = 0xFFFFFFFF;
MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[1] = 0xFFFFFFFF;
MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[2] = 0xFFFFFFFF;
MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[3] = 0xFFFFFFFF;
MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[4] = 0xFFFFFFFF;
MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[5] = 0xFFFFFFFF;
MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[6] = 0xFFFFFFFF;
MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[7] = 0xFFFFFFFF;
MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[8] = 0xFFFFFFFF;
MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[9] = 0xFFFFFFFF;
MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[10] = 0xFFFFFFFF;
MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[11] = 0xFFFFFFFF;
MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[12] = 0xFFFFFFFF;
MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[13] = 0xFFFFFFFF;
MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[14] = 0xFFFFFFFF;
MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[15] = 0xFFFFFFFF;
MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[16] = 0xFFFFFFFF;
MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[17] = 0xFFFFFFFF;
MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[18] = 0xFFFFFFFF;
MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[19] = 0xFFFFFFFF;
MPCBB_Area_Desc.AttributeConfig.MPCBB_LockConfig_array[0] = 0x00000000;
if (HAL_GTZC_MPCBB_ConfigMem(SRAM3_BASE, &MPCBB_Area_Desc) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN GTZC_S_Init 2 */
/* USER CODE END GTZC_S_Init 2 */
}
Solved! Go to Solution.
2026-01-26 7:04 AM
Jocelyn,
the problem was, that in the file partition_stm32h562xx.h the SAU was enabled for some reason. This file was out of my scope. After disabling SAU, the problem disappeared.
Best regards,
Stefan
2026-01-26 1:46 AM
Hello @JungerGott ,
I'm sorry, I don't understand your point. You seem to have a working setup.
Best regards
Jocelyn
2026-01-26 7:04 AM
Jocelyn,
the problem was, that in the file partition_stm32h562xx.h the SAU was enabled for some reason. This file was out of my scope. After disabling SAU, the problem disappeared.
Best regards,
Stefan