Skip to main content
Associate III
November 19, 2024
Question

How to use yolov8 on STM32H747

  • November 19, 2024
  • 13 replies
  • 3319 views

Hi,

 

I have successfully ran and trained the models in modelzoo but I would like to use a larger model with yolov8 for higher resolution.

 

It was mentioned in another post that yolov5 and above is not compatible with ST chips at the moment.

 

In any case can how can I use a previous model let's say v4? The available models seem to be:

st_ssd_mobilenet_v1
ssd_mobilenet_v2_fpnlite
st_yolo_lc_v1
tiny_yolo_v2
 
What would the .yaml file look like. Can I just use the .tflite file from yolov4 and use one of the yolo derivatives from the above list?
 
Alternatively, can I increase the input matrix on the available models to be larger than 416x416?
 
I am using the h747 disco board.
 
thanks
This topic has been closed for replies.

13 replies

Julian E.
ST Technical Moderator
November 19, 2024

Hello @dogg,

For the moment, as you said, only the following models are available for object detection:

st_ssd_mobilenet_v1
ssd_mobilenet_v2_fpnlite
st_yolo_lc_v1
tiny_yolo_v2
 
To deploy it, you can look at this configuration example:
 
Simply put the path to the .tflite model you want to deploy.
 
Regarding input size, you can change it, but you will need to retrain the model:
  • for tiny yolov2 type the input size should be a multiple of 32,
  • for st__yolo_lc_v1 the input size should be  a  multiple of 16.
  • the correct input shapes are 192, 224, 256 for the ssdv1

  • 192, 224, 256, 416 for ssdv2

In the yaml, in the training part, you have a input_size field.
 
 
 
Have a good day,
Julian
​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
doggAuthor
Associate III
November 20, 2024

When I choose 1024x1024 for input size, I get a self.input_shape_list = None at line 296 of tiny_yolo_v2_preprocess.py

 

thanks

Julian E.
ST Technical Moderator
November 20, 2024

Can you share your user_confi.yaml please?

 

When you say 1024x1024, you mean something like that?

input_shape: (1024, 1024, 3)

 

Julian

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
doggAuthor
Associate III
November 20, 2024
general:
 project_name: COCO_2017_person_Demo
 model_type: tiny_yolo_v2
 #model_path: C:/Users/Haris/Desktop/stm32ai-modelzoo/object_detection/pretrained_models/ssd_mobilenet_v2_fpnlite/ST_pretrainedmodel_public_dataset/coco_2017_80_classes/ssd_mobilenet_v2_fpnlite_100_416/ssd_mobilenet_v2_fpnlite_100_416_int8.tflite # C:/Users/Haris/Desktop/stm32ai-modelzoo/object_detection/pretrained_models/st_ssd_mobilenet_v1/ST_pretrainedmodel_public_dataset/coco_2017_person/st_ssd_mobilenet_v1_025_256/quantized_model.tflite
 logs_dir: logs
 saved_models_dir: saved_models
 gpu_memory_limit: 12
 global_seed: 127

operation_mode: chain_tqeb
#choices=['training' , 'evaluation', 'deployment', 'quantization', 'benchmarking',
# 'chain_tqeb','chain_tqe','chain_eqe','chain_qb','chain_eqeb','chain_qd ']

# dataset:
# name: coco_2017_80_classes
# class_names: [ aeroplane,bicycle,bird,boat,bottle,bus,car,cat,chair,cow,diningtable,dog,horse,motorbike,person,pottedplant,sheep,sofa,train,tvmonitor ] # Names of the classes in the dataset.
# training_path:
# validation_path:
# test_path:
# quantization_path:
# quantization_split: 0.3

dataset:
 name: bugs # Dataset name. Optional, defaults to "<unnamed>". [nc, mr, wf] #
 class_names: [nc, mr, wf] # [ aeroplane,bicycle,bird,boat,bottle,bus,car,cat,chair,cow,diningtable,dog,horse,motorbike,person,pottedplant,sheep,sofa,train,tvmonitor ] # Names of the classes in the dataset.
 training_path: C:/Users/Haris/Desktop/stm32ai-modelzoo/object_detection/src/bugs/train
 validation_path: C:/Users/Haris/Desktop/stm32ai-modelzoo/object_detection/src/bugs/valid 
 validation_split: 0.2 # Training/validation sets split ratio.
 test_path:
 quantization_path: C:/Users/Haris/Desktop/stm32ai-modelzoo/object_detection/src/bugs/quant
 # quantization_split: # Quantization split ratio.
 seed: 123 # Random generator seed used when splitting a dataset.

preprocessing:
 rescaling: { scale: 1/127.5, offset: -1 }
 resizing:
 aspect_ratio: fit
 interpolation: nearest
 color_mode: rgb

data_augmentation:
 rotation: 30
 shearing: 15
 translation: 0.1
 vertical_flip: 0.5
 horizontal_flip: 0.2
 gaussian_blur: 3.0
 linear_contrast: [ 0.75, 1.5 ]

training:
 model:
 type: tiny_yolo_v2 #st_ssd_mobilenet_v1
 alpha: 0.35
 input_shape: (1024, 1024, 3)
 weights: None
 #pretrained_weights: imagenet
 dropout:
 batch_size: 2
 epochs: 2
 optimizer:
 Adam:
 learning_rate: 0.001
 callbacks:
 ReduceLROnPlateau:
 monitor: val_loss
 patience: 20
 EarlyStopping:
 monitor: val_loss
 patience: 40

postprocessing:
 confidence_thresh: 0.6
 NMS_thresh: 0.5
 IoU_eval_thresh: 0.3
 plot_metrics: True # Plot precision versus recall curves. Default is False.
 max_detection_boxes: 10

quantization:
 quantizer: TFlite_converter
 quantization_type: PTQ
 quantization_input_type: uint8
 quantization_output_type: float
 granularity: per_channel #per_tensor
 optimize: False #can be True if per_tensor
 export_dir: quantized_models

benchmarking:
 board: STM32H747I-DISCO

tools:
 stedgeai:
 version: 9.1.0
 optimization: balanced
 on_cloud: False
 path_to_stedgeai: C:/Users/haris/STM32Cube/Repository/Packs/STMicroelectronics/X-CUBE-AI/9.1.0/Utilities/windows/stedgeai.exe
 path_to_cubeIDE: C:/ST/STM32CubeIDE_1.16.1/STM32CubeIDE/stm32cubeide.exe

deployment:
 c_project_path: ../../stm32ai_application_code/object_detection/
 IDE: GCC
 verbosity: 1
 hardware_setup:
 serie: STM32H7
 board: STM32H747I-DISCO

mlflow:
 uri: ./experiments_outputs/mlruns

hydra:
 run:
 dir: ./experiments_outputs/${now:%Y_%m_%d_%H_%M_%S}
Julian E.
ST Technical Moderator
November 20, 2024

First of all, I think there is an issue here: 

input_shape: (1024, 601024, 3)

Then, is your dataset a public one, can you link it to me if it is the case? I would like to replicate what you are doing, but I don't have a dataset on my pc. 

 

Julian

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Julian E.
ST Technical Moderator
November 20, 2024

Thanks, 

I will take a look.

Julian

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
doggAuthor
Associate III
November 21, 2024

Ok, when I use 608 trained tiny yolo model I get this error while deploying the model:

File "C:\Users\Haris\Desktop\stm32ai-modelzoo\object_detection\src\../../common/deployment\external_memory_mgt.py", line 88, in update_activation_c_code
line = "#define CAMERA_RESOLUTION (" + cam_res + ")\n"
UnboundLocalError: local variable 'cam_res' referenced before assignment

Which does not happen when I use a 416 trained model.

 

thanks

Julian E.
ST Technical Moderator
November 21, 2024

Hello @dogg,

It seems that the model cannot be superior to VGA (640x480) and it doesn't seem to be upscaling on H7.

You could try with an input size of 480x480 (I don't think 640x480 will pass for the model input)

 

If you want to go further, you need to modify the C code yourself to allow for bigger image acquisition (camera drivers + buffers):

  • you need to bypass the python error for the model to be deployed (it can hardcode the CAMERA_RESOLUTION value it needs).
  • Once the C code is generated, modify the camera drivers so that it sends the resolution you need (greater than or equal in width and height to the model's input).
  • modify the defines to match the camera's resolution.

Normally the code is quite readable, there are patterns in the READMEs

 

The limitation for the model to be trained and to be embedded are different.

I contacted the dev team to add better errors.

 

Anyways, it may be better for you to wait a little bit for the next model zoo release and yolov8

 

Julian

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Julian E.
ST Technical Moderator
November 21, 2024

Additionally, if you want to try, I got the information that if you do as follow, it should let you deploy your model (but it was not tested).

 

Before the deployment, try to replace the value of  "AXIRAM", "size" and "value"  in  stm32ai_application_code/object_detection/mempools_STM32H747I-DISCO.json by 0.

 

In theory, this should put all the buffer is SDRAM which should not saturate.

 

Julian

 

 

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.