cancel
Showing results for 
Search instead for 
Did you mean: 

Write An assembly code in spcstudio

nooshin_1382
Associate II
Posted on August 28, 2016 at 10:08

Hi

I want to write some asm instruction in Spc studio but i don't know how can i write these instructions.

if there is exist any sample please let me know about this sample.

Thanks

With Best Regards

Nazerian Vanima
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Erwan YVIN
ST Employee
Posted on August 29, 2016 at 17:08

Hello Vanima ,

The samples are in HAL (*.c , *.s files) in components directories

#if CORE_SUPPORTS_IVORS
/* The core supports IVOR registers, the kernel requires IVOR4 and IVOR10
and the initialization is performed here.*/
#ifdef __ghs__
asm (
''e_li %r3, %lo(_IVOR4) \t
''
''mtIVOR4 %r3 \t
''
''e_li %r3, %lo(_IVOR10) \t
''
''mtIVOR10 %r3''
);
#else
asm volatile (
''e_li %%r3, _IVOR4@l \t
''
''mtIVOR4 %%r3 \t
''
''e_li %%r3, _IVOR10@l \t
''
''mtIVOR10 %%r3''
: : : 
''memory''
);
#endif
#endif

All CPUs are compatible with the Power Architecture VLE instruction set, which supportssome code size reduction. Best regards Erwan