cancel
Showing results for 
Search instead for 
Did you mean: 

Unable to connect to target with SPC5-UDESTK

CLamb.2267
Associate II

Hello,

I'm trying to program a SPC560B64 microcontroller but debugger can't connect to target :

-driver is correctly install (with vcp enable option check)

-all signal (TDI, TDO, TMS, etc...) are correcty route to the debugger.

-target is powered (green LED is ON on UDESTK)

I use SPC5 studio (6.0) to generate executable and UDE STK 5.0 as external debugger (about this when could we have the debugger running directly in SPC5 studio??)

I jnow there is some others post about this but nothing work here and all these post doesn't have response...

Any advise or better a solution?

This discussion has been locked for participation. If you have a question, please start a new topic in order to ask your question
2 REPLIES 2
CLamb.2267
Associate II

So I answer myself, this was an hardware problem my bad.

I've forgot to connect VDD-BV pin to 5V on my board....

Giuseppe DI-GIORE
ST Employee

Thank you for your answer.