cancel
Showing results for 
Search instead for 
Did you mean: 

Target Board not getting programmed from SPC560D-DIS board

harsh2
Associate II
Posted on May 12, 2016 at 13:02

Hi

I am following PLS adpter settings given in User Manual of SPC560D Discovery board to program my target board having SPC560D30L1 mcu, but instead of target board get programmed, the MCU on discovery board is getting programmed always.

Below are the changes we did for PLS adapter mode

J19 - shorted,

s1,s2 kept opened.

TMS,TDI,TDO,TCK,RSET,VDD,GND pins of  target baord MCU connected to TMS,TDI,TDO,TCK,RSET,VDD,GND pins of Discovery board. 

screen shot attached of Debugger software

Pls advise

#flash-programming #spc560d-dis #-
This discussion is locked. Please start a new topic to ask your question.
6 REPLIES 6
Erwan YVIN
ST Employee
Posted on May 13, 2016 at 15:12

Hello Sharma ,

I think that your configuration is ok.

SPC560D Discovery board has D40 mcu.

Did you try to update the configuration PLS into D30 ?

or update the MCU in SPC5Studio Configuration  (D30 Platform Component) (if you use SPC5Studio) ?

the linker file should be adapted according your MCU.

          Best regards

                        Erwan

harsh2
Associate II
Posted on May 19, 2016 at 07:19

Hi  Erwan

Thanks for the response.....

 i am using spc5studio & have updated the MCU in SPC5Studio Configuration as D30.

but still my target board is not getting programmed...

Please advise, what else i need to check(connections or settings).

Regards

Harsh 

Erwan YVIN
ST Employee
Posted on May 19, 2016 at 14:47

Hello Sharma ,

I suspect a driver issue in your case.

Could you send me a pls screenshot ?

Could you check if the PLS Adapter is well installed ?

you should have cf screenshot

the driver should be located in this following directory

c:\Program Files (x86)\pls\UDE 4.2\Driver\

Best regards

Erwan

________________

Attachments :

2016-05-19_144527.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0SH&d=%2Fa%2F0X0000000bZA%2FyilxyhHc9M.F7KyvxjH43KzsZjTikECfa69GcXza72A&asPdf=false
harsh2
Associate II
Posted on May 23, 2016 at 11:07

Hi Erwan

Please find attachment as snapshot of driver installed.

Regards

Harsh

________________

Attachments :

SPC5_studio_driver.jpg : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0SC&d=%2Fa%2F0X0000000bZ5%2FCC1M08wg6Kkx.hplB.G9GBLr2SZwU2r7NgjqMjHGPmo&asPdf=false
Erwan YVIN
ST Employee
Posted on May 26, 2016 at 10:22

Hello Sharma ,

Could you check your device manager on Windows ?

          Best regards

                       Erwan

harsh2
Associate II
Posted on May 27, 2016 at 11:35

Hi Erwan

yes, i am able to find installed driver in device manager of windows.

Regards

Harsh