cancel
Showing results for 
Search instead for 
Did you mean: 

SPC5Studio Build and Debug Problems

evren
Associate
Posted on October 31, 2016 at 12:57

Hello,

I'm new to SPC5Studio environment and experiencing some problems using it. I'll be glad if you can help about the following issues:

1) When I try to create a project using steps

''File->New->C Project->Makefile Project->SPC5 C/C++ Application''

and press to the ''Finish'' button, an error message is shown saying

''Unknown process: com.st.tools.spc5.WizardProcessRunner''

and the created project is empty. When I use the wizard, I can create an example project which I can succesfully generate and build.

2) I'm working on SPC570S-DISP development board. However, I couldn't connect it through the USB port. SPC5Studio doesn't see it as an hardware to which it can load the program code. Debug button on the Activity Wizard is not activated. 

What should I do to make SPC5Studio to connect the SPC570S-DISP hardware using the on-board USB?

Thanks in advance for any help. 

Regards,

Evren
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Erwan YVIN
ST Employee
Posted on November 07, 2016 at 10:35

Hello evren ,

Sorry for the late answer.

1)

you should create a project by the menu ''New ==> SPC5 C/C++ Application

Anyway , i am creating an error report to remove the possibility to create a Makefile project

2) 2 things to check :

First, Could you check if PLS UDE is well installed in your environment ?

SPC5Studio is looking for if the application is installed on Windows environment.

Secondly, could you check if your driver is well installed ?

(cf screenshot)

Best Regards

Erwan

________________

Attachments :

2016-11-07_103335.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006qWJ0&d=%2Fa%2F0X0000000boC%2FCkcgUHIcahr1RMOy8wwacDpheypRX8OI8L9pnMub8uY&asPdf=false