2025-02-11 04:39 AM - last edited on 2025-02-11 05:00 AM by Peter BENSCH
Hi. I have a problem when trying to establish a serial communication from SPC58 to my PC. My device manager only shows SPC58EC-DISP in the "other devices" section.
1. SPC58EC-DISP is connected with USB cable to my PC.
2. I have installed the drivers from the link that was provided in the DKReferenceCode: CP210x USB to UART Bridge VCP Drivers - Silicon Labs.
3. Installed "CP210x Windows Drivers" and "CP210x VPC Windows" and "CP210x Universal Windows Driver"
4. I run the installer, example "CP210xVCPInstaller_x64".
5. When i try to update the drivers to the SPC58EC-DISP in the device manager, windows doesn´t find the drivers.
Kind Regards,
Joona.