2025-01-08 02:30 AM
2025-01-08 03:43 AM
Welcome @GabiPaz-GSP, to the community!
The RESET pin has an internal pull-down. What have you connected externally to the RESET pin?
Regards
/Peter
2025-01-08 04:51 AM
Hi Peter
Thank you, hope that you can help.
1K as pull-up and 10nF to GND.
The 1.2v and 3.3v provided with 2 DC/DC converters.
2025-01-08 05:22 AM
OK, at least externally RESET is obviously wired correctly.
However, RESET is a bidirectional pin whose internal open drain can be activated by various internal sources. As no information on software etc. is currently available, nobody can make a statement.
2025-01-08 06:43 AM
Hi Peter
After some testing,
2025-01-08 07:41 AM
As far as I know, the order does not play a role during power up, you can also switch them on simultaneously.