cancel
Showing results for 
Search instead for 
Did you mean: 

[solved]Pictus input pin selection

270284440
Associate III
Posted on June 25, 2015 at 11:45

Hello,

Please see attached pictures cut from pictus RM0022 page 86.

There are two input fucntion selectable of A[8] pin, SIN, and EIRQ[8].

I read and understand that to select input function , PCR.IBE = 1 must be set,

but how to set SIN and EIRQ ? by configure in PSMI register or

function of SIN and EIRQ are connected internally in the MCU chip?

Thanks so much!

#pcr-pictus
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Erwan YVIN
ST Employee
Posted on July 02, 2015 at 16:11

Hello Chu ,

No need to use PSMI.

IBE to 1 on A[8] is enough to enable SIN_1 and EIRQ_8

SIN_1 and EIRQ_8 are connected in an intrinsic function.

Best regards

                     Erwan

270284440
Associate III
Posted on July 03, 2015 at 03:42

Hi ,Erwan.

Thank you so much!