cancel
Showing results for 
Search instead for 
Did you mean: 

Self-Test Control Unit RAM test type

ivancolla9
Associate III
Posted on January 19, 2016 at 17:06

Good morning,

I have a techincal question regarding the Self Test Control Unit of  SPC56EL60 microcontrollers.

It seems from the documentation that the unit performs various types of self-tests for the micro, including ram memory test (MBIST). I cannot find what type of memory test the unit perform: abraham, galpalt or others? I am misunderstanding the unit capabilities?

Thanks.

#test #stcu #ram
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Erwan YVIN
ST Employee
Posted on January 20, 2016 at 09:42

Hello Ivan ,

I am checking with SOC Functional Validation team.

   Best regards

              Erwan

Erwan YVIN
ST Employee
Posted on January 21, 2016 at 17:03

Hello Ivan ,

Here is the feedback from Verif Team.

1)      MARCH LR14  (Four backgrounds)

2)      Address decoder delay test

3)      Mask Bit test 

4)      csn test

Best regards

                     Erwan

ivancolla9
Associate III
Posted on January 22, 2016 at 10:04

Well, this is all the information I needed.

Thank you very much for the help,

Ivan