Skip to main content
davide23
Visitor II
January 14, 2016
Question

Using two FlexPWM modules with RPC56EL70L5 (SPC56EL70L5)

  • January 14, 2016
  • 1 reply
  • 707 views
Posted on January 14, 2016 at 10:48

Hi,

I am evaluating the use of RPC56EL70L5 to control two BLDC motors, using a FlexPWM module for each motor.

The datasheet of the SPC56EL70L5 states that the second FlexPWM is not connected to the pins of the package - the RPC56EL70L5 datasheet is not explicit about.

Is there a way to connect the second module (FlexPWM_1) to the output pins?

Any workaround?

Thanks, dave
    This topic has been closed for replies.

    1 reply

    Erwan YVIN
    ST Technical Moderator
    January 21, 2016
    Posted on January 21, 2016 at 18:18

    Hello Dave ,

    Sorry the RM is not clear.

    There is no FlexPWM1 on EL70.

    ''The pulse width modulator module (FlexPWM) contains four PWM channels, each of which

    is configured to control a single half-bridge power stage. One module is present in LQFP144

     

    package. Additionally, four fault input channels are provided per FlexPWM module.''

                                 Best regards

                                                     Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.