cancel
Showing results for 
Search instead for 
Did you mean: 

Running code without debugging (SR5E1-EVBE7000P)

kucerapavel
Visitor

Hello,

I'm trying out examples for the SR5E1-EVBE7000P development board. I use StellarLINK to implement the code on the flash and when I run it via RESUME the code runs. But if I execute Terminate and want to run the code without StellarLINK, e.g. by turning the development board power off and on or using the reset buttons, the code doesn't run. I think I forgot something fundamental. Can I ask someone for help? Compared to e.g. the SPC58EC-DISP, where I also tried StellarLINK, I uploaded the code and after turning the board power back on, the code runs automatically. What should I set up on the Stellar microcontroller so that it also runs the code when the SR5E1-EVBE7000P board power is turned on.

Thank you

Pavel

0 REPLIES 0