2022-01-14 10:28 PM
Hi,
I am using SPC584B70E3 and I want to configure some of the inputs as an ICU. However, the SPC5Studio Limits the ICU for eMIOS0 Channels 0-7 only. I cannot configure PE[0] (eMIOS0 Channel 11 or eMIOS1 Channel 13) as ICU for instance. In the Reference Manual these channels have the ability to be configured as SAIC (Single Action Input Capture) but I do not understand how that is done through SPC5 Studio.
Can you help me with configuring PE[0] as an Input Capture as an example?
Thanks for the help,
2022-01-16 11:56 PM
Hello,
you can open the PinMap editor:Right click on pad 13 (PE[0]) and selec the source you want (emios0 channel 11 or emios 1 channel 13)
then save you pinmap, close it
save your configuration and rebuild all.
Best Regards,
-Olivier
2022-01-17 12:03 AM
Then I am looking to the awnser about the SAIC ...
2022-01-17 12:16 AM
I am sorry if I did not explained my issue more clearly. I know how to set a pin as an eMIOS channel, this is not what I am asking.
If you go to the eMIOS Settings (under Low Level Drivers Component) you can see that only eMIOS0 Ch0-Ch7 are allowed to be configured as ICU. However, in the Reference Manual I can see that more eMIOS channels have the SAIC functionality. I am asking if there is a way to set a different eMOIS Channel as ICU.
2022-01-17 12:30 AM
Your question was perfectly good. I just not found the answer yet.
You are right, it seems the current driver only implements the channels 0 to 7.
I will ask for Driver team support to be able to answer you as soon as possible.
BRs,
-Olivier
2022-01-17 4:46 AM
I had the confirmation that current Low Level Driver do not support more that the 8 first channels of emios0 to be configured in SAIC mode.
Then you will have to use one of supported channels (ch0 to ch7).
Best Regards,
-Olivier