2021-09-15 2:33 AM
Hi everyone,
I am using an AEK-MCU-C1MLIT1 development kit to in and output PWM, which work at least for EMIOS0 channel 0 output on pin PD15 of the SPC582B60E1 processor.
Nevertheless, it is not easy to comprehend, which group and channel number in the SPC5Studio Low Level Driver Wizard corresponds to the UC0-UC31 pins of the processor. According to RM0403 on page 752, the different channels support different modes.
Here as a picture for easy reference:
So far so good. That's why I planned using pins UC13,UC14 and UC15 as IPWM inputs and using UC16 as OPWFMB.
In the configuration wizard groups 1-3 only allow OPWMB or OPWMT mode. And on the group 0 channels, IPWM is not a selectable option.
So my questions:
After reading the RM0403 and the datasheet of the processor itself, I still don't know how to set it up or if that is even possible.
Thanks in advance for an answer.
Best regards,
Christopher Seifert
Solved! Go to Solution.
2021-09-16 7:11 AM
Hello ,
Maybe , you can update the drivers to support IPWM
inplug low level driver and add implement IPWM configuration.
Best regards
Erwan
2021-09-16 7:11 AM
Hello ,
Maybe , you can update the drivers to support IPWM
inplug low level driver and add implement IPWM configuration.
Best regards
Erwan
2021-09-21 5:53 AM
Hello Erwan,
thank you very much for the answer and the insight.
I tried to at least make the IPWM input work on eMIOS0 Ch 2 and created a little example project with channel 0 PWM output externally linked to the channel 2 input.
With the icu width callback reading icup->width I get the following output over UART:
012437<\n>
032365<\n>
052293<\n>
006685<\n>
026613<\n>
046541<\n>
000933<\n>
020861<\n>
040789<\n>
060717<\n>
015109<\n>
035037<\n>
054965<\n>
009357<\n>
029285<\n>
049213<\n>
003605<\n>
This does not look like PWM width measures, but more like overflowing counter.
My new questions:
In the attached icu_pwm_test_count project I calculated the difference of last width value with the new width value. This leads to pretty constant output of period length. Changing the input PWM ratio does not change the pwmWidth value.
I hope somebody may have had the same problems while getting IPWM to work. Thanks for any new insight.
Let me know, if I should start a new thread for this topic.
Best regards,
Christopher Seifert
2021-09-22 1:45 AM
Hi Christopher,
the relation between the eMIOS channels and the PWM low level driver channels is summarizing in the pictures that you can find in the document contained in the folder spc582bxx_low_level_drivers_component_rla/doc within your SPC5Studio test application.
As you can see from the picture, the eMIOS channels 8, 16 and 24 are not available (because there are used as counter for the other channels within the same group). In the current version of the driver for the channels of Group 1, 2 and 3 only the modes OPWMB and OPWMT are supported. Instead, for the channels of the Group0 only the modes OPWFMB (PWM) or SAIC (ICU) are supported.
Regards,
Luigi
2021-09-27 5:16 AM
Hi Luigi,
thank you very much for your support.
I managed to replicate most of the code I need to activate channel 13 as IPWM input.
But I get no counts as if the counter input is not working.
Thanks in advance for any new insight in this topic.
Would be great, if the LLD would support not only PWM output setup, but also the other modes.
Best regards,
Christopher
P.S.: I am not able to open the .chm file in Windows 10. Still figuring out why...