2021-09-17 2:00 AM
Hi,
I am working with SPC58xx, SPC5Stuido 6.0, Windows 10 and I am trying to deploy the code onto the board with UDE 5.0.
Although I've read all the topics about these issues I still can't connect to target.
The drivers have been installed properly and the Load VCA settings are enabled.
What else can I do to make it work?
Thank you!
Solved! Go to Solution.
2021-09-29 1:48 AM
Issue has been resolved. Micro was fitted in the incorrect position.
2021-09-23 5:30 AM
I've installed UDE 5.2 and tried with that one and still doesn't work. The adapter board is SPC58xxDPT176S. The micro is SPC58EE48E7.
The target configuration file is automatically selected in SPC5Studio 6.0 as SPC58NE84. Will this be a problem?
2021-09-29 1:48 AM
Issue has been resolved. Micro was fitted in the incorrect position.