2019-03-15 7:33 AM
* Unhandled exceptions handler for core 0.
*/
.align 2
.weak _IVOR0, _IVOR1, _IVOR2, _IVOR3
.weak _IVOR4, _IVOR5, _IVOR6, _IVOR7
.weak _IVOR8, _IVOR9, _IVOR10, _IVOR11
.weak _IVOR12, _IVOR13, _IVOR14, _IVOR15
.weak _IVOR32, _IVOR33, _IVOR34
.weak _unhandled_exception0
.type _unhandled_exception0, @function
_IVOR0:
_IVOR1:
_IVOR2:
_IVOR3:
_IVOR4:
_IVOR5:
_IVOR6:
_IVOR7:
_IVOR8:
_IVOR9:
_IVOR10:
_IVOR11:
_IVOR12:
_IVOR13:
_IVOR14:
_IVOR15:
_IVOR32:
_IVOR33:
_IVOR34:
_unhandled_exception0:
se_b _unhandled_exception0
Solved! Go to Solution.
2019-03-18 7:52 AM
Hello ,
The handle interruption are in this file (OSAL Component)
SPC56ELxx_RLA IRQ Test Application for DiscoveryPlus\components\spc56elxx_osal_component_rla\lib\src\ivor.s
You can update it by using the patch mode mecanism
Best regards
Erwan
2019-03-18 7:52 AM
Hello ,
The handle interruption are in this file (OSAL Component)
SPC56ELxx_RLA IRQ Test Application for DiscoveryPlus\components\spc56elxx_osal_component_rla\lib\src\ivor.s
You can update it by using the patch mode mecanism
Best regards
Erwan