cancel
Showing results for 
Search instead for 
Did you mean: 

How to get double wire CAN from SPC5?

PSing.5
Associate II

SPC5Studio asks for a TX and RX pin. I selected CAN 1 TX and RX pins and connected them to CAN 2 RX and TX pins I chose (I tried all manner of connections). I am trying to get CAN 2 to send a message. On the output I see a 0 to 5 V signal instead of 0 to 2.5 V and another of 2.5 to 5 V. How do I get two wire CAN? I think I am missing a concept here, can someone please help me.

I am trying to use SPC560B discovery board.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
PSing.5
Associate II

To anyone reading this in the future, the answer to my question was the SPC56 DIS board does not come with a transceiver to produce a CAN_H and CAN_L.

View solution in original post

1 REPLY 1
PSing.5
Associate II

To anyone reading this in the future, the answer to my question was the SPC56 DIS board does not come with a transceiver to produce a CAN_H and CAN_L.