cancel
Showing results for 
Search instead for 
Did you mean: 

Hi, Hi, My setup: SPC560Pxx_RLA SWT Test Application for Discovery uC: SPC560P50L3 IDE: SPC5Studio 5.8.1 This problem occurs when emulator links. Tu 21.04.2020 16:07:54.541, Error, Core::PowerPcInstr, could not access 0x00000000

Lde.815
Associate II

Our program can run when connected to the debugger, but it can't run automatically when unplugged and recharged. What's the problem?

This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
Erwan YVIN
ST Employee

Hello ,

Do you use PLS Debugger or TRACE32 debugger ?

have you flashed your software ?

Could you check your jumpers ?

Best Regards

Erwan

Lde.815
Associate II

Thank you!

Thank you!

  • The board I used was designed by myself, and there is no problem with the reset electricity.
  • The emulator I use is spc5-udestk-eval.
  • To make sure my program is working properly.
  • An error occurs whenever the emulator links to the board.
  •  

Kind regards

0693W000000X3EWQA0.png

Giuseppe DI-GIORE
ST Employee

It is a matter of emulator configuration. Check the configuration files.

Thank you�?

  • Since it is not clear for me to use it for the first time, could you please tell me how to configure it in detail?Or do you have any recommendations?
  •  
  • As shown below, what is the reason for this?(i.e. Error, Core::PowerPcInstr, could not access 0x00000000)0693W000000X3EWQA0.png

Kind regards