2021-06-28 12:19 PM
I am attempting to get the GHS compilier to build with SPC58NG dev kit and have switched the Build settings to below
I have updated the project to include the path and commented out the error statement
ifeq ($(GHS_PATH),)
export PATH := C:\ghs\comp_202114\$(PATH_SEPARATOR)${PATH}
# $(error Please specify a valid path into GHS_PATH for ccppc (GHS) compiler)
endif
and it will compile but then include some strange error that doesn't really help. Is there any setting I need to fix it looks to be something in the linking process.
Solved! Go to Solution.
2024-07-02 08:43 AM - edited 2024-07-02 08:45 AM
TBH this looks circular, adding to the PATH for executables / tools
export PATH := C:\ghs\comp_202114\$(PATH_SEPARATOR)${PATH}
Surely you want to be exporting GHS_PATH, not PATH, as presumable used elsewhere in the scripting or INCLUDE / LIB paths, etc. Or that GHS_PATH exists from the outset in your installed environment.
2021-06-28 01:20 PM
>>compile but then include some strange error that doesn't really help
Says the linker failed because it can't find a symbol/function to bind with.
Either you're missing a source, or object file, or you have some #ifdef level exclusion of code you actually need, but isn't supplied for the GHS tools.
Perhaps start by figuring out what symbol it is choking on, a partial .MAP or linker output? Increase verbosity level if appropriate.
2021-06-29 08:12 AM
Yeah okay it was missing a callback that didnt bother gcc.
On another note every time I regenerate something, the makefile gets regenerated and I have to rewrite the fix in the makefile.
I have added ghs to my path variables on my machine and also in the project. Any work arounds for this?
ifeq ($(GHS_PATH),)
$(error Please specify a valid path into GHS_PATH for ccppc (GHS) compiler)
endif
2024-07-02 08:43 AM - edited 2024-07-02 08:45 AM
TBH this looks circular, adding to the PATH for executables / tools
export PATH := C:\ghs\comp_202114\$(PATH_SEPARATOR)${PATH}
Surely you want to be exporting GHS_PATH, not PATH, as presumable used elsewhere in the scripting or INCLUDE / LIB paths, etc. Or that GHS_PATH exists from the outset in your installed environment.
2024-07-10 02:34 AM
Yes , it is in Windows Preferences , you should add the GHS_PATH in your environment