cancel
Showing results for 
Search instead for 
Did you mean: 

get "Error: Unable to find component plugin" when generate application code in SPC5STUDIO

sdrad
Associate II

Hi there

I'm working on a spc5studio project which one of my friends has worked on it. when I open the project in spc5studio, I get the following error message:

Error: Unable to find component plugin named 'com.st.tools.spc5.components.platform.spc560bcxx'.

Please try to install it from SPC5 market place.

Neither can I generate application code nor I can compile my application via SPC5Studio.

I couldn't find any plugin called 'com.st.tools.spc5.components.platform.spc560bcxx' in internet. what is the problem?

thank you all

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Erwan YVIN
ST Employee
2 REPLIES 2
Erwan YVIN
ST Employee

Hello sdrad ,

You should install the corresponding device from

http://download.spc5studio.com/updates/

Best regards

Erwan

sdrad
Associate II

Hi Erwan

thanks for your response. There was some other plugins that were needed to be installed. I found them in the market place section in help menu and when I tried to install them I encounterd some errors saying that the requested URL is invalid(or something), after so many failed attempts I realized that I must install plugins from the "Help/Install New Software …" and not in marketplace section. It looks as if the market place section have some bugs and nothing can be installed from marketplace. take a look at SPC5STUDIO market place in help menu...