cancel
Showing results for 
Search instead for 
Did you mean: 

GCC compile and flash code

gp73
Associate III

Is it possible to compile the application only with Gcc (free) so do not use GHS or Hightec and flash and run the compiled code?

I can tolerate that this compiler is not efficient as those not free.

This discussion has been locked for participation. If you have a question, please start a new topic in order to ask your question
1 ACCEPTED SOLUTION

Accepted Solutions
Erwan YVIN
ST Employee

Yes , it is possible for you to use gcc (free) for SPC5 Family

The compiler is available on the update site (SPC5Studio Update site)

http://spc5tools.spc5studio.com

you should download from SPC5Studio Tools suite

Best regards

Erwan

View solution in original post

1 REPLY 1
Erwan YVIN
ST Employee

Yes , it is possible for you to use gcc (free) for SPC5 Family

The compiler is available on the update site (SPC5Studio Update site)

http://spc5tools.spc5studio.com

you should download from SPC5Studio Tools suite

Best regards

Erwan