cancel
Showing results for 
Search instead for 
Did you mean: 

Error in the test application??? SPC5Studio

Daniele Mirri
Associate II
Posted on March 21, 2017 at 17:07

I'm using the test application 'STM test Application for discovery'  and also if i never used it, when i want to compile it i have this 3 errors:

FMPLL-IN has a value (0) out of range: [4000000,64000000] configuration.xml /SPC560Bxx_RLA STM Test Application for Discovery FMPLL-IN Problem

FMPLL-VCO has a value (0) out of range: [256000000,512000000] configuration.xml /SPC560Bxx_RLA STM Test Application for Discovery FMPLL-VCO Problem

XOSC has a value (0) out of range: [4000000,16000000] configuration.xml /SPC560Bxx_RLA STM Test Application for Discovery XOSC Problem

Can someone help me??

Does someone knows where are those variables and which are the correct values??

Many thanks.
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Erwan YVIN
ST Employee
Posted on March 22, 2017 at 10:35

Hello Daniele , 

You have chnaged the default settings.

You can use SPC560Bxx Clocktree in the test application to check your clockpoint.

anyway, please refer to the RM for the permitted value. (Cf Clock Chapter)

  Best regards

                 Erwan

View solution in original post

1 REPLY 1
Erwan YVIN
ST Employee
Posted on March 22, 2017 at 10:35

Hello Daniele , 

You have chnaged the default settings.

You can use SPC560Bxx Clocktree in the test application to check your clockpoint.

anyway, please refer to the RM for the permitted value. (Cf Clock Chapter)

  Best regards

                 Erwan