cancel
Showing results for 
Search instead for 
Did you mean: 

EEPROM overflow bigger than 256 bytes

sonerb
Associate II

Hi,

I always take an error "EEPROM_ERROR_FLASH_PROGRAM" while I was trying to write some data on EEPROM.

So, I debugged and realized It returned an error in verify stage.

I give uint32 WriteBuffer[100] and It makes 400 bytes.

In verify stage EEPROM driver is using a counter that the data type is uint8. So, It means just 256 bytes can be verified.

But there is no limit control on the eeprom_write function and no warning for about this.

  uint32_t actualsize;
  uint16_t idsize;
  uint64_t buffer;
  uint32_t buffaddress;
  uint8_t counter;
  uint8_t i;
  uint32_t returnvalue;
  uint32_t address;
  uint32_t idaddress;
  uint32_t alignedbytes;
  uint32_t notalignedbytes;
  uint32_t nuomofcycles;
  uint32_t tempsource;
  uint8_t invalidateid;
 
.
.
. 
 
 /* Verify written data */
  address = eepromp->config->blockConfig[eepromp->currentBlock].startAddr + eepromp->config->blockConfig[eepromp->currentBlock].size
      - eepromp->freespace;
  address += 16U; /*point to data */
  for (counter = 0; counter < size; counter++) {
    if (FLASHREAD8(address) != EEPROM_READ8(tempsource)) {
      return EEPROM_ERROR_FLASH_PROGRAM;
    }
    tempsource++;
    address++;
  }
.
.
.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0